List of Contributions

⚙ Mark Emeott

Contact Details

⚙ Mark Emeott


My Content

1 to 20 of 48 total
Posted By ⚙ Mark Emeott May 19, 2026 09:07:46 AM
Found In Egroup: Emulate3D Software
\ view thread
The new V6.0 Allen-Bradley Velocity Drive Aspects no longer function with the legacy Core Conveyor Motor and instead require use of a Motor Aspect. As a result, the Core Conveyor's built-in Encoder won't function in this configuration. To enable encoder functionality while using a Drive Aspect, add ...
Posted By ⚙ Mark Emeott May 12, 2026 04:23:46 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi, No we don't have any plan to add Kinetix Drives to the catalog. For CIP Motion Drives, the recommended approach is to use Studio 5000's Axis Test Mode feature in Logix V35+ to simulate the position changing and then map the ActualPosition tag to a Visual + Property in E3D. Axis Test Mode ----- ...
Posted By ⚙ Mark Emeott May 12, 2026 02:10:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi, I wanted to let you know that the Allen-Bradley Velocity Drives catalog V6.0 is now available as a Prerelease on Package Explorer in E3D 2026, and now provides an Armor PowerFlex 350 Drive. Documentation is available at: Allen-Bradley Velocity Drives 6.0 --------------------------------- ...
Posted By ⚙ Mark Emeott May 05, 2026 10:18:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Tyler, The E3D site has a basic Knowledgebase guide with an Errors section, but your exception is a C# compiler error: https://store.sim3d.com/knowledgebase/errors Your specific exception mentions the "AB_Digital\_3dControlPanelsExtensions.cs" script, which is part of the Allen-Bradley Module ...
Posted By ⚙ Mark Emeott Apr 10, 2026 02:09:50 PM
Found In Egroup: Emulate3D Software
\ view thread
No, we're not working on an integration with COMAU robot programming software, nor is one planned. Thanks! -------------------------------------------
Posted By ⚙ Mark Emeott Apr 10, 2026 09:28:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Yes, we've been working on this drive and making major improvements to the Allen-Bradley Velocity Drives Catalog for quite some time. Changes will include: Adding a new Armor PowerFlex 350 Drive that supports basic Safety Features (Safe Torque Off, Timed Safe Stop 1, Safety Inputs/Outputs). Automatically ...
Posted By ⚙ Mark Emeott Mar 17, 2026 12:35:00 PM
Found In Egroup: Emulate3D Software
\ view thread
I don't know why the Robot IO Tags aren't able to be wired correctly in your model. Logically, a RO would be an input into the wiring diagram (Read From PLC in the IO Browser) and a RI would be an output from the wiring diagram (Write To PLC in the IO Browser). Unfortunately, we can't troubleshoot ...
Posted By ⚙ Mark Emeott Feb 25, 2026 10:35:00 AM
Found In Egroup: Emulate3D Software
\ view thread
The description for this property is incorrect. In Linear Physics loads will only travel down the centerline. I've put in a request for our development team to update the description to denote the property only applies when using Planar Physics. -------------------------------------------
Posted By ⚙ Mark Emeott Feb 24, 2026 09:28:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Please send in your model or an example model to: Emulate3DSupport@rockwellautomation.com Unfortunately, we can't debug most issues with just screenshots or videos. We need to be able to replicate the problem in order to figure out what's going wrong and then resolve it. Thanks! ---------------- ...
Posted By ⚙ Mark Emeott Feb 16, 2026 09:09:21 AM
Found In Library: Emulate3D Software
Posted By ⚙ Mark Emeott Feb 16, 2026 09:09:00 AM
Found In Egroup: Emulate3D Software
\ view thread
There was a bug in the early Wiring Catalog V3 prereleases that could cause some of the Widgets to not calculate the correct value. And even after upgrading to a later version, the model will require manual intervention to fix the problem. Open your model and make sure it's upgraded to the latest Wiring ...
Posted By ⚙ Mark Emeott Feb 05, 2026 10:43:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Dynamic Joints are ideal for what you've shown in that video. I'd highly recommend using these for the retainer forks. If not, then you'd have to come up with some scripting... maybe enabling & disabling the physics of these retainer forks to allow the loads to pass thru whenever you deem it possible. ...
Posted By ⚙ Mark Emeott Feb 05, 2026 10:24:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Perhaps the Sensor is being blocked by more than 1 load whenever it's not working, so the OnBlockedLogic doesn't execute because there's already a blocking load. You should add a print statement to your QL to see if the event is even executing and what load is triggering it. Also, look at the ...
Posted By ⚙ Mark Emeott Feb 05, 2026 09:35:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Suryan, I think you've misunderstood the purpose of the Engage Forum. It's intended to be a place where users ask questions and share insights on using the Emulate3D software, and E3D personnel can chime in too to be helpful. The Engage Forum isn't the proper support channel to use for bug reports ...
Posted By ⚙ Mark Emeott Jan 29, 2026 09:30:00 AM
Found In Egroup: Emulate3D Software
\ view thread
I'd recommend trying to delete one of the Modules you're having issues with from the Scene, and then re-adding it using the right-click method in the IO Browser. When it's added this way, there's no chance for any of the settings to be incorrect. If you're still having trouble, then please create a ...
Posted By ⚙ Mark Emeott Dec 12, 2025 10:30:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Just to be clear on the versioning of the CAD Is The Model (CITM) releases: 1.0.97 added Unwind/Rollover/Modulo and Jogging functionality to the Advanced Positon Controller. Also, a new Indexing Controller was introduced. 1.0.98 adds a new Proximity Sensor aspect that creates a configurable Cylindrical ...
Posted By ⚙ Mark Emeott Dec 12, 2025 10:13:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Load Creators have an OnLoadCreated event that executes immediately after a load is created. You could use this event to set the Load's Kinematic property to True using QL or C#. Below I've used QL: -------------------------------------------
Posted By ⚙ Mark Emeott Nov 26, 2025 03:14:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi, I went ahead and marked up the FANUC CRX-25iA Robot this afternoon and uploaded it to Package Manager. Thanks! p.s. Lots of new robot were added to Package Manager over the last year or so. The Emulate3D What's New in 2025 slide deck mentioned all the additions. ---------------------- ...
Posted By ⚙ Mark Emeott Nov 21, 2025 11:03:00 AM
Found In Egroup: Emulate3D Software
\ view thread
No, after moving the devices under the Ethernet, you'll then be able to download to the Echo Processor at 192.168.1.3, and then Emulate3D will be able to create a CIP1 connection with this Processor. This is what I've been doing for several years now. -------------------------------------------
Posted By ⚙ Mark Emeott Nov 21, 2025 10:51:20 AM
Found In Egroup: Emulate3D Software
\ view thread
It's not working for you because your IO is routed through the EN2T card. FT Logix Echo doesn't emulate EN2T cards nor do any bridging, it only only emulates PLC Processors. For CIP Class 1 connections to be successful, the networking setup has to exactly match the real-world setup. So, to make it ...