List of Contributions

@ndy

Contact Details

@ndy


My Content

1 to 14 of 14 total
Posted By @ndy Sep 28, 2023 02:47:00 AM
Found In Egroup: Automation Control
\ view thread
I'm along the same thought path as you Phillip that the device cant be directly controlled but the safe link network and I need to use the safety controller for dump valve control Thanks for your reply Andy ------------------------------ @ndy ------------------------------
Posted By @ndy Sep 27, 2023 06:16:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, i have a question regarding the new guard link system as far as i understand this is a device based system, you start with a string of taps and these taps are defined as nodes (last node has a terminator plug fitted) each tap is connected to a single device, this sounds simple if ...
Posted By @ndy Jul 27, 2023 02:46:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi i have a Kinetix 5500 drive where i require 2 registration sensors and a home switch. with the Kinetix 5500 drive you have 2 inputs available and these inputs can be selected as the functions DI1 - Home & Registration 1 DI2 - Registration 2 When using the Home & registration ...
Posted By @ndy Jul 14, 2023 03:13:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you fuzzy, i understand safety is a sensitive topic but you may be surprised how many people just refuse to discuss it directly hence my post on the forum. i understand your points and appreciate you sharing the links so i can look into it furthur. Andy ------------------------------ ...
Posted By @ndy Jul 14, 2023 03:08:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you Brian, you have clarified things and pointed me in the direction where i can look up more information to help my understanding which is exactly what i needed to get my head around this. Andy ------------------------------ @ndy ------------------------------
Posted By @ndy Jul 11, 2023 01:48:00 AM
Found In Egroup: Automation Control
\ view thread
Hi All when using a two hand control function in a safety PLC you have 2 sensors that provide the 2 safety inputs. in all the documentation that i have seen these sensors normally have 1 NC & 1 NO contacts, i assumed that the reason for this was so a positive change in state is seen for each ...
Posted By @ndy Jun 28, 2023 04:44:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Sean Your suggestion sounds like a good option to allow a station to accept any tool and recipe control as you suggest would be vital. by having a recipe containing the tuned parameters your covering mechanical differences with the tool, i like that. do you think the same approach would ...
Posted By @ndy Jun 28, 2023 02:35:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Vincent Thank you for your reply, i have seen some information on RAKB regarding the changing of parameters that may be useful. changing parameters directly may be the way to go with a single station i.e if i had Station A and Tool A & B If i wanted to expand the scope to cover an ...
Posted By @ndy Jun 19, 2023 05:25:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks fuzzy logic, that worked a treat ------------------------------ @ndy ------------------------------
Posted By @ndy Jun 19, 2023 05:21:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have a servo that operates a module on a machine and this module is not always used on all products. if the module (but not the servo) was removed when not in use and potentially an alternate module fitted, would it be possible to have 2 sets of parameters for the same servo? Could ...
Posted By @ndy Jun 15, 2023 10:36:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi I currently have a VM with Rockwell Studio5000 v29 & v35 installed if i open a project that is using v29 i am unable to add a new powerflex drivemodule i get the follwing error failed to create module. class not registered Anyone any ideas? its a new installation that ...
Posted By @ndy Jun 15, 2023 01:52:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Vincent looking into the history of the design it originally had K6000 drives so this would explain why it remained in the K5500 configuration that it had when i started looking at this which aligns with your comment, i will need networked safety so K5500 will be the way to go. thank you ...
Posted By @ndy Jun 13, 2023 11:11:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Vincent The reason i must migrate is due to component availability In Rockwell Automation Publication KNX-RM009F-EN-P - March 2022 it does state that MPL motors can be used, The current 5700 system i have uses a hardwired enable and MSO/MSF commands I am not sure of the reason ...
Posted By @ndy Jun 13, 2023 08:03:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi I have a requirement to migrate kinetix 5700 drives onto the 5500 platform, initially it looks pretty straight forward but the 5700 drives have a configurable input setup as an external enable, unfortunately this enable input is not available on the 5500 drives. Both models of drives are ...