List of Contributions

nmeistrup

Contact Details

nmeistrup


My Content

1 to 20 of 50+ total
Posted By nmeistrup Jun 09, 2026 12:04:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Mihallo, New series 2080-L50E... & 2080-L70E... can manage Class 1 connections. No Safety. See chapter 8 to know what is new feature: Micro830, Micro850, and Micro870 Programmable Controllers User Manual - April 2026
Posted By nmeistrup Feb 02, 2026 11:17:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Martin, All notes about boot problems suggest to review the DC power and to restore the factory image. For example, these notes BF30950 - PanelView Plus 7 Performance series B: booting up to grey screen & BF23099 - PanelView Plus 7: various boot issues- Current last revisions are: ...
Posted By nmeistrup Dec 03, 2025 02:05:00 AM
Found In Egroup: Automation Control
\ view thread
OOhhh, bad luck. may be SD card is more "rapid" to engage it. If not, no solution, the module should be sent it to repair, to remake the boot sector. -------------------------------------------
Posted By nmeistrup Dec 02, 2025 01:23:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Alan, If powering it up with the keyboard and pressing F1 doesn't work, the other way is powering it up with a firmware SD or USB card, better with same revision than original firmware. If it works, then you can upgrade it to desired rev. Could you follow the pages 131 to 134 of this ...
Posted By nmeistrup Nov 12, 2025 05:32:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Luke, Any of our panels support indexing tag reference. This is the culprit of error code. You can manage the indexing in Logix controller code, presenting an auxiliar tag on the panel, that it will be filled in each searching with the Recipe number. Alternatively, for recipes, you ...
Posted By nmeistrup Nov 12, 2025 12:00:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Alan, This case usually is related with a complex Communication Setup, that it is being happening from V10 and next. The solutions are explained in this technote BF17620 - PanelView Plus 6 & 7 frozen with message: FactoryTalk View ME Station is shutting down. If you don't have ...
Posted By nmeistrup Oct 23, 2025 11:52:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Singh, 5069 IO family requires the Series 5x80 controllers. As well as all IO families starting by 50xx catalog numbers (5034, 5069, 5094). Preface chapter in User Manual shows it (page 5): Compact 5000 EtherNet/IP Adapters - User Manual. Publication 5069-UM007 I hope this helps ...
Posted By nmeistrup Sep 26, 2025 02:03:00 AM
Found In Egroup: Automation Control
\ view thread
Hi John & Blake, First, sorry for delay, this week was terrible. In my opinion, if the heat/cool is managing right for your application, I wouldn't do something more on it. Input tags and Status tags are only managed in NT8 by the bit 15 of config tag, because the module only has ...
Posted By nmeistrup Jul 18, 2025 01:41:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Jin, This document suggests to replace by Cat n# 2711P-T6C21D8S in page 15. It requires that your panel only communicates with 1 controller (PanelView Plus 7 Standard cannot set 2 shortcuts). The same MER file will work in new panel. If your panel communicates with 2 or more controllers, ...
Posted By nmeistrup Jun 25, 2025 12:31:00 AM
Found In Egroup: Automation Control
\ view thread
Sorry, I forgot it: CTM module doesn't spend a slot and it doesn't declare in the IO Configuration tree, so any change in the ACD project. It is 12mm width, as well as all modules.
Posted By nmeistrup Jun 25, 2025 12:19:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Awadi, Yes, 1734-OE2C might work very hot in cabinets without forced ventilation. To avoid the problems with output current and hardware degradation, you can use same solution than with old safety modules: putting between OE2C modules 1734-CTM (common terminal module) to separate them, ...
Posted By nmeistrup Jun 12, 2025 12:13:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Hi ECCO, From TechSupport service, we have seen many systems working like you want it. No problems to apply it. Embedded port acts at 1GB if it is connected to a managed switch (4-pair cable) . It might transfer 2000 HMI messages/second, at maximum, assuming no IO messages. Rockwell ...
Posted By nmeistrup May 29, 2025 10:04:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Arunkumar, I reviewed the technote and the Release Notes, and Engineering ensure that rev 8.014 solves the error. PanelView 800 rev8.014 & CCW V23.00 Could you remake the CHA file, and download it to the panel with new revision? Alternatively, to re-flash the panel with same ...
Posted By nmeistrup May 21, 2025 12:26:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Greg, You can use CMP instruction in all Logix controllers to compare 2 STRINGs, same LEN. Page 327 of manual below. Also with 5069-L3xxER and 1756-L8xE controllers you can use EQ (old EQU), same restriction. Page 322. Logix 5000 Controllers General Instructions - 1756-RM003
Posted By nmeistrup Mar 11, 2025 09:13:11 AM
Found In Library: Advanced Software
Posted By nmeistrup Mar 11, 2025 09:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Natalia, It might be a Kepserver issue. The only information that we have noticed is the problem to read array elements. See the attached PTC article. It might help to you. Kindest regards,
Posted By nmeistrup Mar 07, 2025 12:04:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Nuncio, Please, uninstall CCW and clean the computer, deleting the next folders & registers QA34332 - Connected Components Workbench Cleanup Procedure Then reboot the computer and install last version of CCW V22.00
Posted By nmeistrup Feb 27, 2025 09:31:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Nikolas, The version is that Release notes shows for V15.100: Windows10 IoT Core Services 1809 v10.0.17763.1757. This software is a closed OS. It doesn't allow external access to download applications, patches or upgrades. If Microsoft suggests a patch for this system, it will ...
Posted By nmeistrup Feb 27, 2025 09:18:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Tim, The common way to get the filename in Recipes ActiveX is to set one String ingredient with the name. As well as the FileName is a required connection to send/receive to the controller, you can add an ingredient StringXXX with this tag from the controller. For more information ...
Posted By nmeistrup Jan 08, 2025 04:00:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks Galayda. The implicit message is intended to send/receive the basic information of a drive: command/reference and status/feedback. To read many parameters, the explicit messages are useful, and they are the same than before. Old Micro850 LC50 works better in Modbus/TCP than Ethernet/IP, ...