List of Contributions

Varadan

Contact Details

Varadan


My Content

1 to 5 of 5 total
Posted By Varadan Jun 30, 2026 12:56:47 PM
Found In Egroup: Automation Control
\ view thread
Thank you for the explanation!
Posted By Varadan Jun 30, 2026 11:50:05 AM
Found In Egroup: Automation Control
\ view thread
Hi Phillip, I will look into this. However, if the issue was cabling wouldn't the issue be consistent rather than appearing randomly. Also, when I try to connect from a computer to the port from a computer with a new cable, I am unable to ping it which is why I felt this was a port issue rather than ...
Posted By Varadan Jun 29, 2026 01:21:00 PM
Found In Egroup: Automation Control
\ view thread
The firmware version is 34.011 and cabling and connectors appear solid in the cabinet. I believe the physical connection is good because the link light was solid green, which means stable physical connection according to the documentation.
Posted By Varadan Jun 22, 2026 11:52:00 AM
Found In Egroup: Automation Control
\ view thread
I am running a CompactLogix 5480 PLC, sometimes randomly the communication will drop over the B1 port even though the A1 and A2 port communications are intact. Even when trying to connect a computer directly to the B1 port and setting the IP address of the computer to be on the same network I am unable ...
Posted By Varadan Jun 10, 2026 03:35:00 PM
Found In Egroup: Automation Control
\ view thread
I see on Compact Logix 5480 manual that there is a Windows 10 IOT OS that you can access through the DisplayPort and peripheral connections. However, when I plug in my monitor to that DisplayPort connection I am getting no signal. Are there any additional steps that need to be performed to interface ...