List of Contributions

Mihajlo Baić

Contact Details

Mihajlo Baić


My Content

1 to 20 of 50+ total
Posted By Mihajlo Baić Sep 03, 2026 11:54:13 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I am not sure that I've seen anywhere something like that. I guess that you will need to wait for FTDS desktop (i guess it will use FT echo for simulation) I can imagine it will work like that. Or if you have PLC, use FT Remote Access with VPN option, that could work, I've done it before. ---- ...
Posted By Mihajlo Baić Aug 31, 2026 04:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Design time netlogic is not visible to "outside" by default so I am not sure can you reach it by any other means. I was doing some rubbish things by writing directly to YAML, but I really advise you NOT to do it. Maybe you can take a look at the here (click me) They made a MCP server by using C# script ...
Posted By Mihajlo Baić Aug 31, 2026 02:13:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am not sure, i don't deal with C#, for me it is unknown topic. I rely only on finished and built in functions. For this csv import/export script, you need to drag and drop script from library to the NetLogic folder in left side of FT Optix (Project view tab). Then you need to make one KVC in converter ...
Posted By Mihajlo Baić Aug 31, 2026 01:25:28 AM
Found In Library: FactoryTalk Optix
Posted By Mihajlo Baić Aug 31, 2026 01:25:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Your csv format is bad, as I expected. Take a look at the attached file, it will work like this. ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 31, 2026 12:57:08 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Can you post the csv file ? ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 28, 2026 10:37:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I haven't dealt with this, but I'm intrigued. So if you unlock AOI import tags, set everything up in Optix and then lock AOI again it is working fine? It does not lose connection to those tags? ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 28, 2026 10:34:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I don't see anything regarding that in release notes. But I wouldn't be surprised if it was changed, in order to deload CPUs by default settings. Anyway, if you need it at 100ms, it is definitely better to set it yourself than leave to default. EDIT: This happened in 1.7.0 so, maybe in this fix ...
Posted By Mihajlo Baić Aug 28, 2026 05:23:39 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Did you include https://yourLink ? I mean, 99% you did, but.. You must have https://www.rockwellautomation.com/ for example if you'd want to use the link from web browser in Optix. ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 27, 2026 01:29:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I think it is not possible, since it is in-browser thing, already, not just due to Optix. I guess you need to limit that by using IT infrastructure, firewall rules etc.. EDIT: Or maybe you can control the URL by some netlogic script, to make a "whitelist" which would check if the link is on whitelist ...
Posted By Mihajlo Baić Aug 27, 2026 01:05:13 AM
Found In Egroup: Automation Control
\ view thread
Yes, for example 5069-IF4IH and 5069-OF4IH. But in Flex5000 you have analog safety card, while in others you don't. Again, it depends on the small details, what do you need, how much space do you have/want to use, wiring. ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 26, 2026 11:39:00 AM
Found In Egroup: Automation Control
\ view thread
It depends how many IOs you have, firmware of you PLC (because of IO platform support). Compact5000, Flex5000 and PointMax should be more or less very similar to same in most of their capabilities. Flex5000 with larger IO density can help to "squeeze" in bigger number of IO. Also wiring of IOs is ...
Posted By Mihajlo Baić Aug 26, 2026 11:23:23 AM
Found In Egroup: Automation Control
\ view thread
Ah.. I guess that is logical but I cannot find any confirmation. RTC idea came from this image: ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 25, 2026 04:15:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, Yeah, good try, i've read those, thanks. I've tried few of other manuals but no luck, finding somethin that I would interpret as an clear answer. Those kinda talk more about general safety time and hardware (module) definition settings, not about the safety period VS discrepancy in DCS instruction ...
Posted By Mihajlo Baić Aug 25, 2026 02:37:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I'd like somebody to explain to me how does the Logix work in this case: Lets say I have a Safety task with a period of 20ms, and lets say it takes 3ms to finish that task, and I have a DCS instruction with discrepancy time 110ms. How does the PLC evaluate the 110ms? Does that mean that I ...
Posted By Mihajlo Baić Aug 24, 2026 05:35:40 AM
Found In Egroup: FactoryTalk Optix
\ view thread
How are you trying to animate it in Optix? Post more details. Are you using Advanced SVG Object? I sucessfully changed the color of your svg in both emulator and web presentation. ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 17, 2026 12:48:31 PM
Found In Egroup: Automation Control
\ view thread
Check this kb Article There is a known bug. But, I'd say you are already doing it by the "workaround" workflow as you have described... ------------------------------ BR, Mihajlo ------------------------------
Posted By Mihajlo Baić Aug 15, 2026 02:40:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Yes, I was drawing on a locked polyline object or locked SVG and it just kept going there as a child, took me a while because I wasn't even able to see that it was drawn sometimes, because of the colors, then I'd unlock the parent object and see that i have XYZ objects hidden in there because I was thinking ...
Posted By Mihajlo Baić Aug 14, 2026 03:35:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for the reply. For me, it seems pretty unnaturally since I've locked the element so I'd expect that it is not being able to change, add children and other things, lets say that I'd expect to have a behaviour of "background" from FT View ME. But ok, at least I know what to expect now. Also, ...
Posted By Mihajlo Baić Aug 13, 2026 06:52:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I am using a SVG picture as a background of my screen. When I try to draw some line/polyline it gets assigned to the SVG picture as a child object, even if the SVG itself is locked? Is this normal? How to bypass this behaviour? I need to draw on SVG as it is "static" background for me, so ...