List of Contributions

Tim Wilborne

Contact Details

Tim Wilborne


My Content

1 to 15 of 15 total
Posted By Tim Wilborne Feb 28, 2026 08:26:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
I don't think BF29696 could be it because it works most of the time. The chrome idea is intriguing because I don't have Chrome installed, but it looks like Studio 5000 is installing "Chromium" as CEF judging by the pop up that is happening in 37.02. I think the link is saying the problem, "CefS ...
Posted By Tim Wilborne Feb 27, 2026 09:36:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
I had it happen again and got a decent recording of it. I had updated to 37.02 and the results were subtly different but it did make it semi repeatable. 100% it only happens when I have two copies of Studio 5000 open and when I have opened a module properties with an image in each. Right ...
Posted By Tim Wilborne Feb 18, 2026 05:19:00 AM
Found In Egroup: Automation Control
\ view thread
Siemens also has the LCCF_CIPClient and LCCF_CIPServer that allow you to read and write in either direction. -------------------------------------------
Posted By Tim Wilborne Feb 05, 2026 07:42:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
I did #1 of BF27567 and have had it do it since. I am running 37.01. I'll go ahead and update it. Thank you. -------------------------------------------
Posted By Tim Wilborne Feb 03, 2026 05:20:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Thanks, I know it isn't much to go off of. If I every figure out how to replicate it, I'll update the post. -------------------------------------------
Posted By Tim Wilborne Feb 03, 2026 04:55:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Yes, Logix Designer works as expected. The first time I thought the profile was corrupt and figured I would reload it after class so we worked with it as it was for three days. As long as you didn't open the module properties, you never noticed there was an issue. ---------------------------- ...
Posted By Tim Wilborne Feb 03, 2026 01:02:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Yes but I don't want to waste their time on something I can't repetitively replicate. That's why I figured I would see if anyone else has ran into a similar issue. Thanks for having a look at it. -------------------------------------------
Posted By Tim Wilborne Feb 03, 2026 12:27:17 PM
Found In Library: Networks
Posted By Tim Wilborne Feb 03, 2026 12:27:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
Hi Ron. The lost connection was from me disconnecting last week, it will do it while online. Sometimes by simply closing a module properties then opening it back up. But I can sit here all day and open and close it and it won't happen :) Nothing in the event viewer for RSLinxNG.exe. FactoryTalk ...
Posted By Tim Wilborne Feb 03, 2026 11:47:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
For about a year, I've been having an erratic issue with the Module Properties not displaying on devices that have the image on the right side such as the 1734-AENT. I'm running 37.01, 35.01, and 20.06. I have had it happen in both version 37 and 35. It happens about every 3rd class week and I've never ...
Posted By Tim Wilborne Dec 13, 2025 08:10:00 AM
Found In Egroup: Automation Control
\ view thread
The biggest challenge I see is not thinking long term and taking advantage of Studio 5000's tag based addressing. I look in lots of programs that have tags such as B3_00.0. -------------------------------------------
Posted By Tim Wilborne Dec 12, 2025 05:59:00 AM
Found In Egroup: General Discussions
\ view thread
Roanoke VA -------------------------------------------
Posted By Tim Wilborne Nov 27, 2025 08:05:00 AM
Found In Egroup: Automation Control
\ view thread
That makes sense, temperature would affect a capacitor so it would be hard to state. Thanks. -------------------------------------------
Posted By Tim Wilborne Nov 27, 2025 07:50:00 AM
Found In Egroup: Automation Control
\ view thread
Is there a specification anywhere of how long the energy storage system should keep the time while powered off? -------------------------------------------
Posted By Tim Wilborne Nov 22, 2025 08:37:00 AM
Found In Egroup: Automation Control
\ view thread
This is an extremely well written AOI, I have used it many times. One hitch, if you are like me, you charge in and try to use it then you read the instructions when it doesn't work. Follow the instructions on this one, especially page 6 of either the client or server instructions. You don't import the ...