List of Contributions

Chad Dale

Contact Details

Chad Dale


My Content

1 to 20 of 21 total
Posted By Chad Dale Nov 05, 2026 05:53:14 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Looks like you need to click 400x faster... just kidding 😀. Here is a sample project with a DesignTime NetLogic script that will hopefully get you kickstarted: cdal3/PopulatePointArrayDynamicLinks. Details are in the README. ...
Posted By Chad Dale Nov 04, 2026 06:16:05 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Take a look at FactoryTalk-Optix/FeaturesDemo2: Second version of the famous Features Demo. UI/Screens/Data/XYCharts/WorkspaceArea/Columns/XYChart contains a PointArray variable that drives the three different XY Charts in the demo application. You can create dynamic links to the array elements ...
Posted By Chad Dale Nov 04, 2026 06:01:12 AM
Found In Egroup: FactoryTalk Optix
\ view thread
You need to set Node class to Instance to activate the drop-down menu:
Posted By Chad Dale Oct 30, 2026 01:49:20 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I stood up an air gapped test environment and can confirm what you found. There are a handful of dependencies that the FactoryTalk Optix High Availability Manager attempts to download on air gapped nodes and fails: I'll get a request into the product team, but I don't have any further guidance at ...
Posted By Chad Dale Oct 30, 2026 08:04:10 AM
Found In Egroup: FactoryTalk Optix
\ view thread
This will require NetLogic to close a specific Dialog or all Dialogs. There are examples here: NetLogic_CheatSheet/pages/dialog-boxes.md at main · FactoryTalk-Optix/NetLogic_CheatSheet [ExportMethod] public void CloseMyDialog() ( // Get reference to a specific dialog and close it var myDialog = ( ...
Posted By Chad Dale Oct 29, 2026 08:07:57 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I went back to your original screenshot and noticed you were using SelectedValue changed rather than the native User selection changed event. It's possible it's an order of operations issue. The SelectedValue changed event might be firing before the SelectedItem is truly instantiated. I can't make sense ...
Posted By Chad Dale Oct 29, 2026 07:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Try this:
Posted By Chad Dale Oct 29, 2026 06:53:39 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I'll echo Shane, I suspect this is a misconfiguration in your auto ack/confirm settings, combined with the alarm chattering in the controller. A while back I built a proof-of-concept where the lifecycle of the alarm ends up in a single row in the database. The goal was to build a table schema closer ...
Posted By Chad Dale Oct 23, 2026 05:22:54 AM
Found In Egroup: FactoryTalk Optix
\ view thread
There are a couple options in this sample project: cdal3/OpenDialogBoxAtXYPosition. I prefer Option 2 in that app. I have a reusable Option2OpenDialogAtXYButton (type) consisting of a Panel with a Button and PanelLoader as children to it. The Button NavButton is set to Stretch horizontally and ...
Posted By Chad Dale Oct 16, 2026 05:49:33 AM
Found In Egroup: FactoryTalk Optix
\ view thread
The 1.8.0.555 change log mentions the following: [Runtime] Fixed EURange "Constrain" materialization for VirtualKeyboard. I haven't tested this yet, but the description aligns with what you are describing. Can you test your scenario on 1.8.0.555 and report back here?
Posted By Chad Dale Oct 14, 2026 05:49:52 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I did not take it to the next step and test this in a template. Mine too won't open after you run the script to create the OPCUAClient/TagImporter and save the template. It will however save with just the script to create the two nodes. The difference in my script and what you described is you do not ...
Posted By Chad Dale Oct 14, 2026 05:13:24 AM
Found In Egroup: FactoryTalk Optix
\ view thread
FactoryTalk-Optix/FeaturesDemo2: Second version of the famous Features Demo has an example of a Trend on a Report.
Posted By Chad Dale Oct 13, 2026 08:11:06 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Understood. I tested your same method, and it appears the project fails to open because of the variable pointing to the OPC UA tag import type. I had a simple project with only a variable pointing to it, and it would not open. I managed to get to work using the following snippet: public class DesignTimeNetLogic ...
Posted By Chad Dale Oct 13, 2026 06:20:35 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Trend objects work in a Report on the OptixEdge, so you are not wasting your time. I suspect it is a configuration error. Can you provide screenshots of the Trend configuration and the Datastore Table you are trying to query?
Posted By Chad Dale Oct 13, 2026 05:46:16 AM
Found In Egroup: FactoryTalk Optix
\ view thread
If your goal is to create OPC UA Client nodes from an OPC UA Server programmatically, your best path is likely to use the 'Runtime configuration' in the properties of the OPCUAClient Node. The following sample app has an example configuration of this: FactoryTalk-Optix/FeaturesDemo2_M2M_Client: OPC/UA ...
Posted By Chad Dale Oct 13, 2026 05:25:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
It looks like a syntax error in your URL. There is no underscore or space in your "Window1" name. The string after "windows/" needs to be an exact match for your Window name. Try this URL "http://localhost:8443/windows/Window1"
Posted By Chad Dale Aug 26, 2026 05:24:50 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you everyone for raising this one. I recreated it as well and reported it to Technical Support yesterday, so we can get it in the queue to address it.
Posted By Chad Dale Aug 20, 2026 06:35:45 AM
Found In Egroup: FactoryTalk Optix
\ view thread
The time to execute a pull is proportional to the git diff size. Larger change = Longer time to pull. With the project having 3.5M nodes, it's likely that your git diffs are also very large. The developers are aware of this and actively looking at ways to improve pull performance for these larger projects. ...
Posted By Chad Dale Aug 15, 2026 09:38:46 AM
Found In Egroup: FactoryTalk Optix
\ view thread
If you can replicate on a blank project, please give technical support a call, so we can assign a ticket and trace it to resolution. I'm happy to take a second look if you share it here as well.
Posted By Chad Dale Aug 14, 2026 05:35:50 AM
Found In Egroup: FactoryTalk Optix
\ view thread
The only related line item in the release notes from 1.7.3.39 that I see is Fixed memory leaks in the ExternalVariableSynchronizer and alias leftovers in the UI session object It's difficult to say if that is related or not but does indicate some change that may be related. My recommendation ...