List of Contributions

Angelo

Contact Details

Angelo


My Content

1 to 13 of 13 total
Posted By Angelo Feb 23, 2026 08:56:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I am trying to engineering units to the new recipe list: If figured if I drilled down to the individual entry fields I could use a string-formatter to do something like this: Unfortunately that only works if the dynamic link direction was display only. If it bi-directional ...
Posted By Angelo Feb 20, 2026 09:46:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
This did resolve the issue. Thank you. ------------------------------ Thanks, Angelo ------------------------------
Posted By Angelo Feb 20, 2026 08:25:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I made a fresh 1.7 program and just placed a couple displays on the main windows and imported the tags I am having trouble with to see what happens. I run into the same issue. Here is a copy of the new program with the same problem with the UNitId missing from engineering units. ------------------------------ ...
Posted By Angelo Feb 20, 2026 08:24:49 AM
Found In Library: FactoryTalk Optix
Posted By Angelo Feb 20, 2026 08:11:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Yea, I just went through and changed them do what you have above in 1.7 to get them to work again. What I linked above is how they were in 1.6 and they were working in a final version of a program in a machine like that. ------------------------------ Thanks, Angelo ---------------------- ...
Posted By Angelo Feb 20, 2026 07:42:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Removing Float as the alias kind did not help. While working through the errors in my optix program another thing that seems to not work any more is math in dynamic links. In 1.6 multiplying the width by negative 1 as I have above worked just fine. ------------------------------ Thanks, Angelo ...
Posted By Angelo Feb 19, 2026 02:31:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I forgot to add a picture of the warning in my original post. Here it is: ------------------------------ Thanks, Angelo ------------------------------
Posted By Angelo Feb 19, 2026 02:21:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I made a custom display that uses a string formatter to display a analog value and its units. This was working fine until I updated the project to 1.8 this morning. Now all I receive is a warning message that I have an Invalid or incomplete configuration because I am missing UnitID under EngineeringUnits ...
Posted By Angelo Jan 08, 2026 09:07:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, In FTOptix I am using a number animation targeting the left margin of a message to move it across a screen. I am trying to set a bit using a transitioned event for the left margin. In this way I was going to use said bit to trigger the animation of the next message. The issue I am running ...
Posted By Angelo Oct 29, 2025 09:26:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I am using a transparent text box as an overlay for numeric entry and would like to change the height of it once it has been clicked on. Is there a way to look at the status of an objects focus such that I can use it as a condition in a expression evaluator? ------------------------------ ...
Posted By Angelo Oct 17, 2025 09:07:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
This is exactly what I was looking for thanks! ------------------------------ Thanks, Angelo ------------------------------
Posted By Angelo Oct 16, 2025 01:49:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I am trying to replicate a panelview HMI screen in optix. I am having trouble figuring out how to make a numeric entry field that has min/max and units. If I use a spinbox I have the min/max but I can't seem to get a string formatter to work with it. If I use a text box I can use the ...
Posted By Angelo Jan 12, 2022 10:00:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, I was hoping someone would be able to shed some light on an issue I ran into. I have a machine that is using a powerflex 755 as a servo motion axis. I ran into an issue where the drive had a fault 91(Pri VelFdbk Loss) which showed up in the PLC motion axis fault list as "Feedback Data Loss Factory ...