List of Contributions

VB6 talking to

Contact Details

VB6 talking to


My Content

1 to 15 of 15 total
Posted By VB6 talking to Apr 21, 2024 07:20:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
QA13495 - PowerFlex 750 Series Drive Fault F8 [Heatsink OvrTemp] (TechConnect) QA22323 - PowerFlex 750 Series: IGBT Temp vs Heatsink Temp Linkified the technote references - MJC
Posted By VB6 talking to Apr 17, 2024 07:18:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Indeed, you can modulate the motor current limit using the parameter 0:422[Current Limit 1]. However, be aware that as soon as the current reaches this current limit, there will be a compromise on your commanded speed up to the immobilization of the motor. You can observe bit 0 [Current Limit] of parameter ...
Posted By VB6 talking to Apr 13, 2024 06:56:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Reference: Programming Manual - PowerFlex 750-Series AC Drive Page 318: Fault Description. Page 98: to disable the fault. You might need a braking resistor if you want to achieve the programmed deceleration. If you already have a braking resistor, make sure that P426 [Regen Power Lmt] is not ...
Posted By VB6 talking to Mar 19, 2024 07:20:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
The PowerFlex 755 has its own Torque Proving / Lifting algorithm. Please refer to document PowerFlex 750-Series AC Drives Programming Manual Look at page 452, onward. "PowerFlex 755 Lifting/Torque Proving TorqProve™ is a PowerFlex® 755 drive feature that is intended for applications where proper ...
Posted By VB6 talking to Jan 17, 2023 07:35:00 AM
Found In Egroup: Legacy
\ view thread
https://literature.rockwellautomation.com/idc/groups/literature/documents/td/1336f-td001_-en-p.pdf Page 42 to 47 Series A and B are compatible. ------------------------------ VB6 talking to ------------------------------
Posted By VB6 talking to Aug 05, 2022 04:42:00 AM
Found In Egroup: Legacy
\ view thread
Bonjour Russel, Noise can affect the volatile memory. Here is how and why. Each time you make an edit, the firmware is calculating a new memory checksum value and stores it as a reference value in a register. That is the same for a SLC, a PLC-5 and a ControlLogix. Before each program scan, ...
Posted By VB6 talking to Mar 30, 2011 11:44:00 AM
Found In Library: Networks
Posted By VB6 talking to Mar 30, 2011 11:44:00 AM
Found In Egroup: Networks
\ view thread
Internal LED description for troubleshooting channels. Wait for the ORANGE - ORANGE code (Start of one munite cycle) Then follow throught the cycle using this chart. ##HL31
Posted By VB6 talking to Mar 30, 2011 11:27:00 AM
Found In Egroup: Networks
\ view thread
Do the pull test with your hands. If one of the connectors pulls off, re-crimp all connectors; adjust the crimp force screw (crimp pliers) to the maximum. ##HL31
Posted By VB6 talking to Mar 30, 2011 05:40:00 AM
Found In Egroup: Networks
\ view thread
Did you use the 1786-CTK ControlNet Coax Tool Kit ? Do a "Pull Test" on each end BNC connectors (black coax trunk line). They must retain a 60 pounds weight, but, if BNC connectora are not correctly installed, ti will be easy to pull off. If possible, replace very short coax lenghts with bullet ...
Posted By VB6 talking to Mar 29, 2011 03:46:00 PM
Found In Egroup: Automation Control
\ view thread
The answer is very simple: NO ! I wish we could! You need to use arrays instead of named UTDs. ##HL38
Posted By VB6 talking to Mar 29, 2011 03:37:00 PM
Found In Egroup: Networks
\ view thread
I had that problem a long time ago. Need more info. Is that appening only at one location (node)? Is it a redundant media network? 1- If you have any serie A RPA, they need to be rev G01 or higher. If not, you can have intermittant blinking red led (and disrupted I/O) 2- Make sure to declare ...
Posted By VB6 talking to Mar 29, 2011 02:38:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
The ground fault is detected by an internal CT around the three output phases. At any point in time, the total current read by that CT must be 0. If not, there is one phase leaking to ground. The trip level is not adjustable. 1- The fault is real: check the output phases unbalance. Check for resistive ...
Posted By VB6 talking to Mar 17, 2010 07:05:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
You need to use the "Min Torq/Spd" mode [Parameter 88, Speed/Torque Mode = Min Torq/Spd] and set the command speed to the maximum speed you don't want to exceed. It must be set higher than the actual speed while pulling the wire. If you have a wire break, the speed loop will take over and regulate ...
Posted By VB6 talking to Jan 25, 2010 04:15:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
A disconnected CT will create an OverCurrent Fault. Check all connections. ##HL33