List of Contributions

Keith Hogan

Contact Details

Keith Hogan


My Content

1 to 20 of 50+ total
Posted By Keith Hogan Jan 16, 2026 08:50:00 AM
Found In Egroup: Automation Control
\ view thread
@Splash, you can do what you want with a text display. Make sure you turn on binding on the Text property (by default binding is off). Then bind the text you want in quotes and use the concatenation operator "+" to concatenate the tag you want. You're seeing all the extra decimal points because these ...
Posted By Keith Hogan Dec 03, 2025 02:18:00 PM
Found In Egroup: Automation Control
\ view thread
Morley, Thanks for the explanation. I think to do what you want, you would need to use the IP address of the panel in your project event and then write the current screen name to a different PLC location depending on which of the 5 project events triggered on the panels. Looking at your screen captures ...
Posted By Keith Hogan Dec 03, 2025 10:13:00 AM
Found In Egroup: Automation Control
\ view thread
Morley, As you suggested, you could use your own button with a Popup Close command instead of using the caption bar. If you want the button to animate a pressed state faster, you can accomplish that with property bindings as described in tech note QA39478. #ViewDesigner Regards, ...
Posted By Keith Hogan Dec 03, 2025 10:08:00 AM
Found In Egroup: Automation Control
\ view thread
Morley, Could we get a little more information about what you are trying to accomplish? What do you mean that you have 5 panelviews in the line? Are you trying to have each PV5000 write their current screen name to the same Logix controller? Regards, ------------------------------ Keith ...
Posted By Keith Hogan Oct 09, 2025 09:44:00 AM
Found In Egroup: Automation Control
\ view thread
Dietrich, This was caused by an anomaly in FTLinx. One possible work-around is to create a new FTLinx ethernet driver just to the PanelView 5000 and do the upload using that driver. That FTLinx anomaly should be fixed in FTLinx 6.50 and later and was also supposed to have been patched in FTLinx ...
Posted By Keith Hogan May 09, 2025 01:47:00 PM
Found In Egroup: Automation Control
\ view thread
Ant, Do you have any other SD cards you could try? Another test you could try would be to save your project as a vpdr in View Designer, copy the vpdr file to the SD card, insert the SD card into the panel, and go to the Load from Media predefined screen to see if the panel can see the vpdr file ...
Posted By Keith Hogan Mar 25, 2025 01:50:00 PM
Found In Egroup: Advanced Software
\ view thread
Harsch, Would the standard controller status indication on the system banner provide you the indication you are looking for? If the PanelView 5000 detects an issue with the controller or cannot communicate with the controller, it will show the controller status indicator: If you press ...
Posted By Keith Hogan Mar 11, 2025 03:38:00 PM
Found In Egroup: Automation Control
\ view thread
Harsch, The PlantPAx team that created the PAI faceplate used visibility to overlay a set of numeric inputs over the numeric displays showing the limit values based on the CurrentUserRole. CurrentUserRole is a system tag used to show the role of the currently logged in user. If you search on the ...
Posted By Keith Hogan Dec 09, 2024 03:35:00 PM
Found In Egroup: Automation Control
\ view thread
Gamze, If that doesn't work, you could try opening a case with tech support. They can help try to duplicate the issue and walk you through gathering any relevant crash dumps to help analyze the issue. Regards, ------------------------------ Keith Hogan View 5000 Software Product Manager ...
Posted By Keith Hogan Dec 05, 2024 03:05:00 PM
Found In Egroup: Automation Control
\ view thread
Gamze, What version of View Designer are you using? Does this happen every time you do a download? Regards, ------------------------------ Keith Hogan View 5000 Software Product Manager Rockwell Automation ------------------------------
Posted By Keith Hogan Oct 16, 2024 09:59:00 AM
Found In Egroup: Automation Control
\ view thread
Harsch, I haven't seen that issue. Maybe there is something with your specific monitor resolution and Windows scaling factor setting? Have you tried running this through tech support? That would be the first step to see if we can find an answer. Regards, ------------------------------ Keith ...
Posted By Keith Hogan Sep 05, 2024 10:52:00 AM
Found In Egroup: Automation Control
\ view thread
E_D, Could you check if your numeric inputs have an initial value defined in View Designer? In other words, they look like this: If so, try putting in a numeric value for the initial value and see if that helps. Like so: Regards, ------------------------------ Keith Hogan View ...
Posted By Keith Hogan Aug 21, 2024 09:34:00 AM
Found In Egroup: Automation Control
\ view thread
Jeff, Have you reported this to tech support? We would like to understand what is happening, and that would be the first step. What other software are you running on that computer? We have seen one other instance of what you are describing with another customer, but after a long investigation, ...
Posted By Keith Hogan Aug 19, 2024 08:45:00 AM
Found In Egroup: Automation Control
\ view thread
Harsch, There is no way to bind the TimeSpan property on the trend. Note that the TimeSpan property just designates how quickly the trend will display real-time data from the tags bound in the trace configurations. Historical data from those tags captured in data logs will display at whatever sample ...
Posted By Keith Hogan Aug 01, 2024 06:53:00 AM
Found In Egroup: Automation Control
\ view thread
Splash, Tech note QA58830 https://rockwellautomation.custhelp.com/app/answers/answer_view/a_id/1125503 describes how to use a project event to set the PanelView 5000 time equal to the Logix controller time. Regards, ------------------------------ Keith Hogan View 5000 Software Product ...
Posted By Keith Hogan Jul 26, 2024 08:17:00 AM
Found In Egroup: Automation Control
\ view thread
Here is a not particularly difficult, but definitely weird control loop I implemented years ago. The customer had an eddy current furnace along a track. At the head of the track, a ram would push a steel ingot onto the track. The ingots would make their way down the track pushed along by the newer ingots. ...
Posted By Keith Hogan Jul 24, 2024 04:51:00 PM
Found In Egroup: Automation Control
\ view thread
E_D, Popups always have the 8 pixel padding since they were not intended to cover the entire screen. Could you perhaps use another screen as your confirmation screen? When your operator presses the button to confirm their choice on the confirmation screen, you could execute a Navigate Backward command ...
Posted By Keith Hogan Jun 21, 2024 12:35:00 PM
Found In Egroup: Automation Control
\ view thread
John, Here is the tech note which gives some considerations for screen switch times: IN9476. Regards, ------------------------------ Keith Hogan View 5000 Software Product Manager Rockwell Automation ------------------------------
Posted By Keith Hogan Mar 19, 2024 08:04:00 AM
Found In Egroup: Automation Control
\ view thread
Just to clarify, you can do all your development in View Designer just using the offline acd file configured as the "Logix Project File" in Project Properties. You only need the "HMI to Controller Path" and "Emulator to Controller Path" to test the project using either a physical controller or an emulated ...
Posted By Keith Hogan Feb 29, 2024 05:03:00 PM
Found In Egroup: Automation Control
\ view thread
Delisle, That looks like a mistake in the manual. The resolution of the 19" PV5510 is 1280x1024. Do you have the publication number and rev of the manual you're using? I can work with our Info Dev people to get that fixed. Regarding sizing of elements on the screen, the trick with the PanelView ...