List of Contributions

Northshore Hero

Contact Details

Northshore Hero


My Content

1 to 12 of 12 total
Posted By Northshore Hero Jul 28, 2026 04:39:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, I'm using FTBatch 18 and believe I've found a bug related to String parameter defaults. When exporting a recipe that contains a String parameter with a default value of a single space (" "), the resulting XML is written as . On import, however, that space appears to be trimmed, leaving the ...
Posted By Northshore Hero Apr 24, 2026 02:48:00 PM
Found In Egroup: Automation Control
\ view thread
@LogicIQ - According to Pedro they had already exported the project to an L5k and imported it back to an ACD. @Pedro Silva - Dynamic Air - I have seen issues like this before. With the leading cause being insufficient user privileges (IE not an administrator), and an antivirus locking a process ...
Posted By Northshore Hero Apr 08, 2026 09:53:00 AM
Found In Egroup: Automation Control
\ view thread
I would like to add some additional information, in hopes that others are able to reproduce it. The minor fault can be triggered without a method call, by toggling the Cmd_ConnectionCheck bit in the raC_Opr_HTTP_Client AOI itself. -------------------------------------------
Posted By Northshore Hero Apr 07, 2026 12:36:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I'm wondering if anyone else has tried using the raC_Opr_HTTP AOI's and not had issues with minor faults. We are using the GET request and are able to receive information just fine from the HTTP server but every single time a request is submitted we get a minor fault. Since the minor fault ...
Posted By Northshore Hero Mar 19, 2025 06:22:00 AM
Found In Egroup: Automation Control
\ view thread
I've seen something similar. Unfortunately for us we will have the echo servers lose the programs even through a normal reboot. We have made it a procedure to turn off the controllers before restarting the server. Then once it restarts, we turn them back on. This will retain the program.
Posted By Northshore Hero Feb 28, 2025 02:21:00 PM
Found In Egroup: Advanced Software
\ view thread
Update on this - there was a tech note released on the issue. The issue is not resolved after just a restart. You need to stop a service otherwise it will happen again. This will only be an issue today. Issues will stop tomorrow. FactoryTalk Directory: FactoryTalk Server and Clients losing communication ...
Posted By Northshore Hero Feb 11, 2025 05:24:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, I was wondering if anyone has had any success with automating the compiling of global objects in FTView SE. This has provided massive performance uplifts when properly used but is easy for people to miss (only a small icon in the top header in view studio). It's really an awesome feature ...
Posted By Northshore Hero Sep 20, 2024 04:19:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I am using the 1756-CFM module for the first time and am wondering how I may go about determining if there is a channel fault or not. Looking at the manual I see the following as an input back to the PLC: I'm stuck trying to figure out how this actually works though. The definition ...
Posted By Northshore Hero Sep 11, 2024 03:54:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi Chip, Given that the issue has tracked you across multiple revisions of PlantPAx config software I am curious if the issue with excel itself. Would it be possible for you to install 64bit excel and run the registry key script shown here: This should be included in the Process ...
Posted By Northshore Hero Sep 11, 2024 09:48:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Chip, Fortunately, / Unfortunately you are not alone with issues regarding this tool. 7.6.3 has had a few bugs that I have already communicated with support on, and they told me they passed it on to the product team. Namely the issue with the templated excel file (for the OPC spreadsheets) and ...
Posted By Northshore Hero Aug 19, 2024 03:06:00 PM
Found In Egroup: Automation Control
\ view thread
Hi GLaDOS, I have done something similar and my suggestion to do this would be to make control strategy library object with a parameter that points to the modules in the IO tree in ACM. This would allow you to not need to modify the Rockwell provided IO module libraries. If you add a parameter ...
Posted By Northshore Hero Jun 27, 2024 10:09:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, I believe that I have found a bug in the Graphics Framework builder that was released with the latest PlantPAx tools. When creating an HMI Application, the tool will create a client startup macro where the HW OrgBus is incorrectly defined. This is shown in the attached image: The ...