List of Contributions

Ryan Murphy

Contact Details

Ryan Murphy


My Content

1 to 20 of 50+ total
Posted By Ryan Murphy Aug 25, 2026 03:49:00 PM
Found In Egroup: Automation Control
\ view thread
Appendix C of the following manual is a good read: https://literature.rockwellautomation.com/idc/groups/literature/documents/rm/1756-rm093_-en-p.pdf . Also a good read: ID: IN41037 | Access Levels: TechConnect Logix Safety Systems Calculations . Technically I suppose neither one directly ...
Posted By Ryan Murphy Aug 25, 2026 08:58:39 AM
Found In Egroup: Automation Control
\ view thread
Hi Pravin Rajha, Can you please provide some more information like part numbers? What controller are you using? Which Prosoft Device are you using? What APL switch are you using? Are you able to ping your other devices? You say you were unable to get the complete data. Does this mean you ...
Posted By Ryan Murphy Aug 21, 2026 11:29:13 AM
Found In Egroup: Legacy
\ view thread
Ah ha! Vindication! I was correct that you cannot download while the adapter is in the scanlist with the network running. ID: QA17615 | Access Levels: TechConnect Editing Flex I/O over a running DeviceNet System ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy Aug 21, 2026 09:53:23 AM
Found In Egroup: Legacy
\ view thread
Hi lingampelly, It has been a while since I had to modify a devicenet network. In a quick offline setup in RSNetworx I had to remove the Flex adapter from the scanlist and re-add it for the amount of input data to update in the scanner's input mapping. I can't remember for sure, but you may have ...
Posted By Ryan Murphy Aug 04, 2026 02:02:37 PM
Found In Egroup: Automation Control
\ view thread
Such information does appear to be available for the Point I/O system. I don't know if anything could be extrapolated from that information: https://literature.rockwellautomation.com/idc/groups/literature/documents/um/1734-um016_-en-p.pdf ------------------------------ Regards, RM -------------- ...
Posted By Ryan Murphy Aug 04, 2026 12:18:36 PM
Found In Egroup: Automation Control
\ view thread
Apparently Rockwell's opinion is summed up here: ID: QA79061 | Access Levels: Everyone The use of 1769 I/O as distributed I/O with 3rd party PLC's TLDR; 1769 is only intended for use with Rockwell PLCs so no information will be provided on assembly instances. ------------------------------ Regards, ...
Posted By Ryan Murphy Jul 28, 2026 11:27:59 AM
Found In Egroup: Automation Control
\ view thread
I already have v38.02 (07/2026) installed, which is even later than v34.05 (12/2025), so I should already be at the latest AOP host, shouldn't I? I think this is indicated by the Core version 32.14.11.0 shown in the screenshot, but maybe I am wrong. A colleague who has v34.01 was able to create ...
Posted By Ryan Murphy Jul 24, 2026 03:17:00 PM
Found In Egroup: Automation Control
\ view thread
I have a program with a L72 v34.013 processor and a few Prosoft modules; one MVI56-PDPMV1 and two MVI56E-GSC. Each of the Prosoft modules appear to be configured in the controllogix rack as Generic modules. Attempting to open one of the Prosoft module properties in v34.03 of Studio5k will, at best, open ...
Posted By Ryan Murphy Jul 13, 2026 02:38:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Steve. To program a ML1400 you would need minimum v8.30 of Logix500. You would need v11 or greater to utilize the password feature introduced in FRN21. They did not add a Series C processor selection in Logix 500, but series C functions the same as series B; just hardware changes, I believe. ...
Posted By Ryan Murphy Jun 24, 2026 01:39:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Kohlman, Can you provide any more details? What firmware revisions are involved? What are the indicators on the COMM card doing? Any error code on the devicenet scanner? What scanner are you using on your network? ------------------------------ Regards, RM --------- ...
Posted By Ryan Murphy May 11, 2026 11:42:00 AM
Found In Egroup: Automation Control
\ view thread
Hello Barreto, This should be interesting reading for you: ID: QA51354 | Access Levels: Everyone Managing the Safety Network Number (SNN) on a Safety Application Hope it helps. ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy May 04, 2026 03:47:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Ah, in that case the 20-750-ENETR or 20-750-ENET2P are your best options, which can be purchased separately. More information available here: ID: QA34443 | Access Levels: Everyone PowerFlex 753: EtherNet Options Hope it helps. ------------------------------ Regards, RM ------ ...
Posted By Ryan Murphy May 04, 2026 12:48:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Just realized your part numbers and the screenshot do not match the title of your post. Which drive are we talking about? 523 or 753? Or other? ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy May 04, 2026 12:43:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi HogueGregPLC, Short answer is that the 523 does not come with ethernet as standard. I think this technote should give you most of the information you seek: ID: QA31864 | Access Levels: Everyone PowerFlex 523, 525, and 527 Comparison and Communication Options Hope it helps. ...
Posted By Ryan Murphy May 04, 2026 12:37:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Rivera, Does this technote cover your scenario: ID: QA16641 | Access Levels: Everyone PowerFlex 750 Safe Speed Monitor Module not running, HIM shows "configuring" ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy May 04, 2026 08:33:00 AM
Found In Egroup: Legacy
\ view thread
Does nothing show up in the S2 bits when this happens? I would guess a processor error occurred that kicked it out of Run Mode. Alternatively it could have lost power and is not configured to go to Run Mode on Powerup. Regards, ------------------------------ Regards, ...
Posted By Ryan Murphy Apr 14, 2026 08:27:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Efremov, See page 165 of manual for default login information: https://literature.rockwellautomation.com/idc/groups/literature/documents/um/20comm-um015_-en-p.pdf See page 43 for instructions on how to reset parameters to default. (Which I hope also means resetting password to default.) ...
Posted By Ryan Murphy Apr 09, 2026 04:01:00 PM
Found In Egroup: Legacy
\ view thread
Hi Lepore, Here is a document with the pinout of the 1756-CP3 cable you could verify against your current cable: https://literature.rockwellautomation.com/idc/groups/literature/documents/in/1756-in046_-en-p.pdf . Are you certain the port on the L61 is configured for DF1? . ...
Posted By Ryan Murphy Apr 02, 2026 09:54:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Well, you'll notice that those two fields you pointed to, Out_LogicCommand and Out_FreqCommand point to specific elements of the data type. Those elements are part of the base data type and don't change so you're good there. This was kind of what I meant by intermediary UDT, the way they are copying ...
Posted By Ryan Murphy Apr 01, 2026 02:26:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Easiest workaround would be to create an intermediary UDT, I suppose. ------------------------------ Regards, RM ------------------------------