List of Contributions

Larriva

Contact Details

Larriva


My Content

1 to 3 of 3 total
Posted By Larriva Jun 10, 2024 01:00:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I'm able to control the drive if I disable the AOI and go through the drive I/O control, see below But I would like to use the faceplate/aoi functionality from the power device library, Whenever I use the AOI to control the drive, the activate and deactivate outputs are just flashing and the ...
Posted By Larriva Jun 10, 2024 09:48:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I cannot control/start a Powerflex 525 with the commands provided by the AOI from the Power Device Library, I set the activate command to high and speed but the drive wont do anything is there something I'm missing? attached image has the code I'm using