List of Contributions

Carlo_G

Contact Details

Carlo_G


My Content

1 to 19 of 19 total
Posted By Carlo_G May 12, 2026 08:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Is the FTRA Local connection free to use or do you need licenses for this? I will surely try this and recommend this to our customers. A lot of customers still want to use a VNC like connection and have local connection or through a VPN. THanks! ----------------------------------------- ...
Posted By Carlo_G May 12, 2026 07:49:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
THanks for the quick answer. RemoteAcces is not an option now since they use different kind of Remote Accesses. FTP is an option if FTPS can be used. BUt not preferred in the future I guess, since you will introduce a new connection way which is not preferred by CRA. v.1.8 would be a good ...
Posted By Carlo_G May 12, 2026 04:29:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Everyone, Since CRA is comming in Europe, our customers want to download a CSV export file remotely through a secure way. Chat and CoPilot give me hints, but they have no idea how to finish it. Lets beat AI. ;-) The standard DataLoggerExport script can create a CSV logfile on the Physical ...
Posted By Carlo_G Oct 31, 2025 09:37:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you very much!! -------------------------------------------
Posted By Carlo_G Oct 31, 2025 06:16:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I saw the new thread coming in almost the same time. This was indeed the answer I was looking for. THanks to Xavier we also could see the Optix connections to the Docker Influx 3.0 DB. Thanks! -------------------------------------------
Posted By Carlo_G Oct 30, 2025 03:52:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I do not know if I can ask you guys this. We want to create a project with the OptixEdge. We can use Optix for the fieldbus communication, poll all data and store this data in a Database and create a UserInterface in Webpage. Docker can be used by the customer to run their algorithm in. Question ...
Posted By Carlo_G Sep 19, 2025 03:31:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you for the tips. We also had a support call at ASEM and they replied that in Codesys communication, there always needs to be a Codesys gateway present in the network. IT seems that with Optix v.1.6.2, there is a Gateway build into the drivers. So We upgraded, changed the Codesys driver and rebooted ...
Posted By Carlo_G Sep 16, 2025 09:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear Forum, Our customer wants to connect an Optix Standard panel to a Schneider LMC 101C controller. We had a correct working OPC-UA connection, but the OPC server takes to much CPU load on the controller side, so we need to change communication protocol. The LMC 101C is based on Codesys. ...
Posted By Carlo_G Jul 24, 2025 02:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Is there a nice way to programm a tooltip for an alarm. So if an operator clicks on an active alarm, that they can get a pop-up to tell what the operator should do in the case of the alarm. Hope you can find some good tips or examples for us. Kind regards, Carlo
Posted By Carlo_G Jul 24, 2025 02:46:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Our customer has an import project for Optix and controllers for us. They are building a very nice optix project, but are looking for a Dynamic way to build a Datagrid list that can be changed lateron. They would like to have 10 string texts for product descriptions prepared, but at this stage ...
Posted By Carlo_G Feb 24, 2025 09:06:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Jennifer, Thank you for this tip. The examples are on a public GIthub location. Along with 90 other examples. https://github.com/FactoryTalk-Optix But this tip I also did not know and could solve my issue even better. THanks! I will try it out. Carlo
Posted By Carlo_G Feb 24, 2025 09:04:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi All, Sometimes the solution is simple. It looks like I just had to press enter after entering a Name for a Pen to add it. I just typed in a new name and clicked on the next parameter. Problem solved!! Try i out. I is a nice demo (when you press enter ;-) ) Carlo
Posted By Carlo_G Feb 20, 2025 09:58:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear Team, My customer wants to use a dynamic way of trending. Adding trends and pens at runtime in a flexible way. This public Github example seems to demonstrate it, but it does not seem to run. I have Optix v.1.5 running and it is automatically upgraded after opening it. But I cannot add ...
Posted By Carlo_G Jan 10, 2025 07:38:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi AutomateSHane, You are correct, there is of course some project history to it. The issue is standarisation in the project. The ASEM 6300 PA is choosen for its mechanical form. Since there is no Optix HMI yet, we choose to use the Windows PanelPC type and run an Optix Runtime on it. This ...
Posted By Carlo_G Jan 10, 2025 03:42:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear team, Our customer is using an ASEM 6300PA Optix panel with Windows 10 IoT LTSC (2019). They want to use an Active Directory fucntion for the User control on the same panel. But since it is not a Windows server edition, they cannot use the Windows Active Directory functionality. For this they ...
Posted By Carlo_G Jan 07, 2025 05:13:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I was reading your question. If you are asking if you can see the panel on FT linx network browser, then the answer would be, no. The Optix panels will not be detectable bij FT Linx since they work different. But if the PLC and HMI are on the same subnet like youdescribed, then the Tags from the HMI ...
Posted By Carlo_G Oct 02, 2024 08:10:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
It's as simple as that. Works as a charme. Thanks!
Posted By Carlo_G Oct 02, 2024 03:15:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi All, I want to invert a Boolean in Optix. The Help file explains that it can be done with an Expression converter by using the ~ sign. See help file: I tried this in Optix on a simple LED function on a Digital Bool Model Var, but it is not working: Any tips ...
Posted By Carlo_G Jun 28, 2024 04:01:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear Team, How can we use #FTOptix as a runtime in a Docker environment? Are special installations needed or is there a container file that can be downloaded to run in Docker? And after it runs in Docker, are NativeEngine and WebEngine both supported? Last part, how can we download an application ...