List of Contributions

Gary Morrison

Contact Details

Gary Morrison


My Content

1 to 8 of 8 total
Posted By Gary Morrison Feb 19, 2022 01:37:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Just to add the info I missed yesterday. I'm using a Micro850 2080-LC50-24QBB. Firmware version 12.011
Posted By Gary Morrison Feb 18, 2022 08:29:00 AM
Found In Egroup: Automation Control
\ view thread
Yeah I tried to attach in a reply email then attached within the rockwell forum
Posted By Gary Morrison Feb 18, 2022 08:13:00 AM
Found In Egroup: Automation Control
\ view thread
I've attached the file. Thankyou
Posted By Gary Morrison Feb 18, 2022 08:12:48 AM
Found In Library: Automation Control
Posted By Gary Morrison Feb 18, 2022 08:07:00 AM
Found In Egroup: Automation Control
\ view thread
I've attached the log file. Thank you
Posted By Gary Morrison Feb 18, 2022 07:45:00 AM
Found In Egroup: Automation Control
\ view thread
Windows 10 version 21H1 (OS Build 19043.1526) CCW ver 13 Full fault message is "Failed to get running image info from controller. See log file C:\ProgramData\Rockwell\CCW\Log\ISaGRAF.ISaGRAF5.Vsx.log for more details." I'm unsure of the controller firmware as I won't be at again until tonight but I did ...
Posted By Gary Morrison Feb 18, 2022 04:37:00 AM
Found In Egroup: Automation Control
\ view thread
Hi fuzzy logic. Thankyou. And thanks for the reply and the link. Yes I've been thru everything on that link (I didn't mention it on my initial post to just keep it short). I got the IT company my company use to go thru it and also do the clean up suggested to make sure it was completely uninstalled before ...
Posted By Gary Morrison Feb 17, 2022 02:15:00 PM
Found In Egroup: Automation Control
\ view thread
Is anybody using USB-C to connect to a Micro850 without any problems? It's been suggested to me that USB-C might not work (I'm using a new Dell XPS13 laptop with only 2 x USB-C connections) so I'm hoping to confirm or rule out this as the cause for my "Failed to get running image info from controller" ...