List of Contributions

Guru Thakkar

Contact Details

Guru Thakkar


My Content

1 to 5 of 5 total
Posted By Guru Thakkar May 18, 2026 12:27:00 PM
Found In Egroup: Automation Control
\ view thread
Sounds like you're using PlantPAX objects on both the panelview and the SCADA, and need "client side" limitations, not at the PlantPAX instance level. Try macros on panelviews that forces the user at the panelview to a "read only" (or user with restricted rights) when the physical input selecton ...
Posted By Guru Thakkar Nov 26, 2025 06:08:00 AM
Found In Egroup: Legacy
\ view thread
MAC won't get "overwritten" if that's what you meant. To merge the tags and comments, export it from the pffline file and import that into the uploafed code file. If there are differences in code, the tags and comments may not make sense though. ---------------------------------- ...
Posted By Guru Thakkar Nov 09, 2025 10:57:00 AM
Found In Egroup: Automation Control
\ view thread
Look into the 1734-VHSC, it has a "capture/latch" input. You can use a common output and wire it to the capture input. Don't use mechanical relay, use opto splitter to split output into 3 signals. -------------------------------------------
Posted By Guru Thakkar Oct 28, 2025 06:25:00 AM
Found In Egroup: Automation Control
\ view thread
Short answer: you need professional/expert evaluation of the situation. Moving IOs "live" is going to be tricky depending on what your system does. It will need a closer look and very careful planning - if that is even possible to do it safely. A few tips below to minimize the downtime, I do not ...
Posted By Guru Thakkar Oct 13, 2025 04:05:00 PM
Found In Egroup: Automation Control
\ view thread
It's a good portal, some trainings do not have labs, but the ones with labs are very useful as there's course work to follow at your own pace. -------------------------------------------