List of Contributions

Marty Walker

Contact Details

Marty Walker


My Content

1 to 6 of 6 total
Posted By Marty Walker Jun 16, 2026 04:33:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Is there a set of documented guidelines or an installation guide for deploying Optix on a Server? I am thinking about topics such as should the Optix development software be installed on the server or should the applications be developed off the server and then 'imported' into the server? If Optix Studio ...
Posted By Marty Walker Apr 10, 2026 08:43:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Rockwell has a sample program on their GitHub related to this topic. Take a look at WPE Sessions Demo at the following link: GitHub - FactoryTalk-Optix/Optix_Sample_WebPresentationEngineSessions: Automation Fair 2025 lab about different Presentation Engines of Optix · GitHub ---------------------- ...
Posted By Marty Walker Mar 16, 2026 04:51:00 PM
Found In Egroup: Automation Control
\ view thread
If an ASEM 6300P-SW0 was originally ordered without a hard drive, can I add a hard drive to the SW0 in the field and put Window 10 IOT on it? Currently the SW0 is functioning as a thin client station, but the desire is to use it as stand-alone industrial computer. ----------------------------- ...
Posted By Marty Walker Jun 05, 2025 11:26:00 AM
Found In Egroup: Automation Control
\ view thread
I'm running into an issue with the French translation of "Result"-which is "Résultat"-on one of the built-in FactoryTalk screens. The problem is that the text box is too short, so the word gets cut off. On all the user-configurable screens, I can adjust the text box size to fit longer translations. ...
Posted By Marty Walker May 29, 2025 08:52:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Thanks Eduard for the quick response. I appreciate it.
Posted By Marty Walker May 28, 2025 01:55:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
The 1783-RA5TGWC4G includes both WIFI and Cellular access. If I have that model, and I choose to not use the Cellular capability, can I still use the WIFI option without purchasing and installing a SIM card? In the manual for the unit (page 6) , it looks like I may have to purchase and install a SIM ...