List of Contributions

Kurt Thayer

Contact Details

Kurt Thayer


My Content

1 to 6 of 6 total
Posted By Kurt Thayer May 17, 2022 08:59:00 AM
Found In Egroup: Automation Control
\ view thread
Fuzzy Logic, I have been in contact with AMCI and they have been very helpful. My key issue has been code execution and/or IO scan times wreaking havoc with the logic. The buffering of input data is already being accomplished, but not the output data. I will have to rework AMCI's AOI to incorporate ...
Posted By Kurt Thayer May 13, 2022 02:42:00 PM
Found In Egroup: Automation Control
\ view thread
All, I see the error in my logic and thinking as I am executing all in a single scan. Obviously this is just junk logic on my part. my production code is misbehaving. I have AMCI 3204 stepper modules that require data to be written to each channel at each step in rapid succession. Due to the structure ...
Posted By Kurt Thayer May 13, 2022 08:09:00 AM
Found In Egroup: Automation Control
\ view thread
I hear what your saying, the issue is after the first execution the first ring becomes false, despite progressing to 20 and 30 and then gags at step 10 due to the timer not becoming false and DN bit becoming false. If what you are saying is true it should be scanning, resetting timer to not done and ...
Posted By Kurt Thayer May 13, 2022 05:12:00 AM
Found In Egroup: Automation Control
\ view thread
So Here is a picture. This picture was taken after starting the sequencer by changing the value from 0 to 10 in order to start. It ran through one cycle as mentioned and as intended, counter incremented but 1 as expected, then sits stuck at the value of 10, with every rung true and not scanning/updating/executing ...
Posted By Kurt Thayer May 12, 2022 10:13:00 PM
Found In Egroup: Automation Control
\ view thread
FWIW, I use multiple vm's with AB, Siemens, GE/Fanuc, and other without issues. I use VMware only. I also only use windows 7/10, no server OS's. Due to complexity and configurations of server OS's I personally feel a server OS is poor choice for a programming terminal. I know AB says it works fine and ...
Posted By Kurt Thayer May 12, 2022 09:47:00 PM
Found In Egroup: Automation Control
\ view thread
1757-L82ES + L8SP partner, on 33.012 firmware on both, using V33 studio is behaving badly in regards to code execution. All code is ladder. This project is a migration from SLC hardware and has been experiencing scan time issues related to the new hardware being much faster. Most old logic has been placed ...