List of Contributions

Hansson

Contact Details

Hansson


My Content

1 to 20 of 21 total
Posted By Hansson Oct 07, 2026 04:02:58 PM
Found In Egroup: Automation Control
\ view thread
Thanks alot, I'll wait for reply
Posted By Hansson Oct 05, 2026 02:01:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, I have a problem with this sensor, it may be the application but I need to sort things out. Manual to the sensor: https://literature.rockwellautomation.com/idc/groups/literature/documents/in/45dms-in001_-en-p.pdf I have eight 45DMS-B8LGT1-D5 that I use the analog output value of. The sensor look ...
Posted By Hansson Apr 28, 2026 08:13:00 AM
Found In Egroup: Automation Control
\ view thread
Opinions on this? To clear the question: The MC1 consist of 2 REED contacts, as far as I've been told this is a well-tried technique and as such a well-tried component. It says in note2 This product has two electrical switching functional channels. The B10d data given for this product is based ...
Posted By Hansson Apr 24, 2026 07:49:00 AM
Found In Egroup: Automation Control
\ view thread
Regarding the 700-HPS relay I see now that I can't use it the way I need to, thanks! The MC1 info is a little bit hard to interpret I think. See above -------------------------------------------
Posted By Hansson Apr 24, 2026 07:37:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks for the answer. I interpred that 1)note as the maximum achievable DC value is achieved with dual channel configuration not that it didn't allow single channel, since single channel dont require DC. Note 1 seems to be about DC. It also says: 2) This product has two electrical switching functional ...
Posted By Hansson Apr 23, 2026 03:25:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, Two questions. Can I use a 440N-Z2NRS1C magnetic non contact switch to a 700-HPS relay? The relay is only 0.7W and it seeems that the magnetic switch is at 200mA (about 5W). But it also say on the switch " Designed for use with specified controllers" (however nonw specified). We currently ...
Posted By Hansson Jun 04, 2025 12:39:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, I understand that, but is it normal to drain the battery on a month of power down? /Tim
Posted By Hansson Jun 04, 2025 01:31:00 AM
Found In Egroup: Automation Control
\ view thread
We have oneMM1 but not programmed to reload so that we can do. Is there a way to disable the RTC? So we can avoid unnecsesarry drain? But do the RTC really drain the battery if the PLC is powered off for 1 month? Can there be any other issues with the PLC that drain the battery?
Posted By Hansson Jun 03, 2025 01:58:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, We have a customer that has a micrologix 1400. They power down the control panel for several weeks at a time and is complaining about battery failure and program loss. As I understand if the battery dies during power off they will loose the program on the PLC? How long should a battery ...
Posted By Hansson Apr 07, 2025 08:30:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, Late reply: On the 800F button it says in the spreadsheet: 1) Products in this library are not specifically intended as safety devices, and the associated data represents reliability data. For this product, any use of the terms MTTFd, B10d, T10d or PFHd does not relate to a failure to ...
Posted By Hansson Jan 28, 2025 01:09:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, Does Allen Bradley provide any easy using switch that has B10d values to use in safety circuits? The 800F series emergency stop button has a B10d value, how about the rest of this series or the 194L line? We currently use a 194L-e12-350X switch for a Hand-0-Auto but the hand mode is now ...
Posted By Hansson Jan 07, 2025 02:39:00 AM
Found In Egroup: General Discussions
\ view thread
Hi, I used to be able to search for a product on the rockwellautomation homepage and be able to go to a product page that told me lead times to my country. Since a couple of weeks back I can't seem to find this, can anyone direct me to the page where this is? /Tim
Posted By Hansson Apr 03, 2024 01:56:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Generally, where can I find HS codes and country of origin on the rockwell homepage? Specifically the 2711P-T7C22D9P ver B /Tim
Posted By Hansson Mar 28, 2024 07:05:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, I recently bought 7 panelviev 7 performance series B as spare parts. I have commisioned six of them, all worked good. The last one I think is broken somehow: After the firmware download the screen got upside down and mirrored. The touchscreen also doesn't respond to where I press. I ...
Posted By Hansson Mar 06, 2024 12:18:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
As I read the technical documentation page 11 is for a 140MP series of MPCB?
Posted By Hansson Mar 04, 2024 01:39:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks, but it doesn't say anything about vertical mounting of 140MT series MPCB
Posted By Hansson Mar 01, 2024 07:27:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I don't find anything in the technical specifications if the 140MT series of MPCB is allowed to be mounted vertically, and if they are allowed can we mount side-by-side or need to consider keeping distance between them. /Tim
Posted By Hansson Feb 12, 2024 02:08:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, Is there any B10d values for 700-HL series? 700-HLT1Z24 to be more specific /Tim
Posted By Hansson Jan 02, 2024 02:29:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, Since my local suppier doesn't get any answers from Rockwell for several months I try here instead. We are using legend plates and more specifically the 194L-A4-350A, 194L-A4-178 and 194L-A4-526. Until recent (some months) they were in silver grey. Now they (some) ship out as regular ...
Posted By Hansson Dec 06, 2023 12:47:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I have found that the 700-K b10d value is the same as 700S-CF. But how about the mechanically linked contacts? Is the 700-K series contacts mechanically linked? If so, is also the front mounted aux. contacts linked? I would like to use the 700-K because of its size but otherwise I will go for ...