List of Contributions

Nickm

Contact Details

Nickm


My Content

1 to 20 of 21 total
Posted By Nickm Jan 27, 2025 04:17:00 PM
Found In Egroup: General Discussions
\ view thread
How can I fix the datetime format to follow my browser's locale?
Posted By Nickm Jan 23, 2025 07:44:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
"A HUGE banner at the top" You mean bigger than the current 300px high one? Discourse forum headers are 66px My post literally starts more than halfway down a 1K monitor :)
Posted By Nickm Jan 23, 2025 06:56:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
It was more a vent rather than a genuine belief that my post could actually result in change... I posted something along the same lines 2-3 years ago obviously with no result ¯_(ツ)_/¯ Should have gone with Discourse... I still have no idea how or if I even can see my forum activity, such as topics ...
Posted By Nickm Jan 23, 2025 06:49:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I would like to suggest an improvement to the current forum structure. Given that this community supports 19 distinct applications, the lack of dedicated sub-categories seems counterintuitive. The current format requires users to sift through irrelevant content for applications they do not use. Also, ...
Posted By Nickm Jan 23, 2025 06:36:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Is there a dashboard or something where I can see what data log models are running? Or otherwise, how can I tell if a data log is running? I can run `DataLogOn ` and check the logs for "...already running" but that's a bit silly.. Also, can I show the running status of the data logs on a view? ...
Posted By Nickm Jun 20, 2023 07:16:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
This seems quite inflexible. It would be great if a lot more of the SVG properties would be made editable to avoid overcomplicating the SVG design process. What would also be great would be able to set the stroke to non-scaling so that whatever size it is, it will always be the width that you set. Otherwise, ...
Posted By Nickm Jun 19, 2023 09:20:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
By magic colour, I mean similar to "magic numbers" in code. In computer programming, a magic number is any of the following: A unique value with unexplained meaning or multiple occurrences which could (preferably) be replaced with a named constant A distinctive unique value that is unlikely ...
Posted By Nickm Jun 19, 2023 07:38:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi @Hobbs , are you able to define standard colours and then use these instead of magic colours? ------------------------------ Nickm ------------------------------
Posted By Nickm Jun 19, 2023 02:10:00 AM
Found In Egroup: Automation Control
\ view thread
One important thing to note here is that (I believe), regarding steps 1 and 10, you're not able to supply a literal string value into the global parameter for the display path. This must come from a string tag, as Fuzzy has demonstrated. ------------------------------ Nickm -------------- ...
Posted By Nickm Jun 18, 2023 06:39:00 PM
Found In Egroup: Automation Control
\ view thread
You should be adding a Goto Display button into the Global Object for your engine itself as per step 3 of Fuzzy's reply. The Parameter List should be set to: `(#1)` Then on the instances of the global object that you've dragged onto your page, you can set the global object parameter values. This ...
Posted By Nickm Jun 15, 2023 08:44:00 PM
Found In Egroup: Automation Control
\ view thread
On the contrary, I don't recommend using parameter files, since you will need to create one for every device. The whole point in using template objects is to get away from having to manually create something for each template, other than the tags themselves. It's been a while since I've used FTV, ...
Posted By Nickm Jun 01, 2023 07:38:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Really appreciate the detailed response! I'm not sure how to quote on this forum.. so forgive the dodgy quotes "However, it is approaching the same caliber as Ignition" This is the platform I come from and have been using for the last 7 years, so that's where most of my questions ...
Posted By Nickm Jun 01, 2023 02:16:00 AM
Found In Egroup: General Discussions
\ view thread
Thanks for the info. The issue however that I can see with tagging is that this is not enforced to be added when creating a topic, so searching for specific-product-related topics is therefore difficult and could result in a large number of unrelated results. ------------------------------ Nickm ...
Posted By Nickm May 31, 2023 08:44:00 PM
Found In Egroup: General Discussions
\ view thread
def thanks(): return "I must be blind :)" ------------------------------ Nickm ------------------------------
Posted By Nickm May 31, 2023 08:39:00 PM
Found In Egroup: General Discussions
\ view thread
How can I format code on this forum? E.g. similar to this on another forum: ------------------------------ Nickm ------------------------------
Posted By Nickm May 31, 2023 08:31:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I'm trying to animate the stroke and fill colours independently in an advanced SVG component, but I can only seem to set both to a single colour. Is it possible to bind to these independently? Also, is it possible to configure other SVG properties like: stroke-width stroke-dasharray ...
Posted By Nickm May 31, 2023 06:52:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Is there a demo project that is available to download that showcases the features of Optix? and more importantly, how to actually do common things in the software? Like (may be different terminology in Optix): creating "tag UDTs" and instances of them creating and using graphic "templates" ...
Posted By Nickm May 31, 2023 06:09:00 PM
Found In Egroup: General Discussions
\ view thread
I'm trying to find how I can show topics only for a particular product, but there only seems to be an "Advanced Software" forum that has topics for every single RA product in existence, and when creating a topic itself, there doesn't appear to be a way to denote what product your topic applies to 🤔 ...
Posted By Nickm Jan 24, 2023 07:46:00 PM
Found In Egroup: General Discussions
\ view thread
Thanks Eileen, I did actually receive an email which I appeared in my spam folder. However, I didn't see anything in the FAQ about seeing notifications within the webpage itself. Is there somewhere in this forum that shows reply notifications? ------------------------------ Nickm -------------- ...
Posted By Nickm Jan 23, 2023 04:05:00 PM
Found In Egroup: General Discussions
\ view thread
I've only just joined and I posted in the Advanced Software community/forum and got a reply last night, but I didn't see the reply show up as a notification anywhere. I only stumbled upon it when I revisited my topic. Are reply notifications shown anywhere? And how can I get reply notifications ...