List of Contributions

Nancy Zupick

Contact Details

Nancy Zupick


My Content

1 to 15 of 15 total
Posted By Nancy Zupick May 01, 2025 11:14:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, I want to explain some things about Arena first before I answer your question. Entity Type is an Element within Arena that defines the entities you create via the Create module or the ones you define via assignments in your logic. The Entity Type information is used in the statistics reporting ...
Posted By Nancy Zupick Jun 19, 2024 11:27:00 PM
Found In Egroup: Advanced Software
\ view thread
Arena Visual Designer does not have an editor for creating .x, .3ds, or .skp files. You will have to look for a third-party tool to create those graphic objects. If you have downloaded the files, you should be able to associate them with the animation for both 3D objects as well as Resources. It is ...
Posted By Nancy Zupick Jun 19, 2024 08:41:00 AM
Found In Egroup: Advanced Software
\ view thread
If you have a specific .x file that you are trying to use in the animation, and it is not working, you can try loading that file into this thread for us to evaluate or you can send it to Arena-Support@rockwellautomation.com for it to be evaluated. Below is a screen capture of an animated object in ...
Posted By Nancy Zupick Dec 20, 2023 09:00:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello Pisaturo, Having read your questions, I am going to recommend that instead of using various Create modules, why not store the sequence of how you want to load orders into the system by reading in the values or updating a variable array that would represent the Part and Quantity ordered. To ...
Posted By Nancy Zupick May 31, 2023 10:00:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, You can find example models for various concepts under the File/Browse Smarts option. ------------------------------ Nancy Zupick ------------------------------
Posted By Nancy Zupick Sep 28, 2022 12:07:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, There are two ways to assign the color of the car, using an Attribute alone or using an Attribute and a Picture (for animation). Define numbers for the available colors: Blue = 1 Red = 2 Purple = 3 Yellow = 4 etc.. Create an attribute that represents the color, a_CarColor and then you assign ...
Posted By Nancy Zupick Sep 23, 2022 09:53:00 AM
Found In Egroup: Advanced Software
\ view thread
This is the example using attributes to indicate failure of inspection and a need for rework. Nancy Zupick
Posted By Nancy Zupick Sep 23, 2022 09:49:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, You can assign any entity's attributes in a number of different ways, the simplest way is to use the Assign module to give them a value. The entity is created and you assign the value. You can overwrite the values that are assigned to attributes at any time. So if an entity passes through a ...
Posted By Nancy Zupick Sep 09, 2022 12:33:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello Brendan, I read your post and I wanted to ask a question. Are you matching same size entities together? For example if you have a part that is 10 cm long and another that is 20 cm long, will they fuse together and be 30 cm? If that is going to occur you will need to compute that new size before ...
Posted By Nancy Zupick Sep 09, 2022 12:32:43 AM
Found In Library: Advanced Software
Posted By Nancy Zupick Jun 27, 2022 11:12:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, Please contact arena-support@ra.rockwell.com, they will provide you with a way to resolve this. The other method to fix it is to repair Office or the Microsoft Access Runtime 2013. The issue has to do with the various different drivers required by not only Arena but other applications on your ...
Posted By Nancy Zupick Jun 27, 2022 11:10:00 AM
Found In Egroup: Installation & Activation
\ view thread
Hello Henning, Please contact arena-support@ra.rockwell.com, they will provide you with a way to resolve this. The other method to fix it is to repair Office or the Microsoft Access Runtime 2013. The issue has to do with the various different drivers required by not only Arena but other applications ...
Posted By Nancy Zupick Jun 27, 2022 10:55:00 AM
Found In Egroup: Advanced Software
\ view thread
Sam, To answer your question, you can assign your furniture (entities) attributes which represent the type of furniture it represents. Generally speaking you can start with a list of the furniture that will be produced in the model scenario and starting with with the number 1, assign them a number that ...