I have a 460 volt, 150hp, 112kw, 172amp, 1.15 sf motor, and a 480volt, 186 amp, 150hp inverter, and a resistance of 4.8ohms at 19200 watts, now my question is what parameters should be moved in the parameters of the variator. I think it is p372, p373, p375, p382, p383, p384, p385, what parameters do ...
|