List of Contributions

JBlumenthal

Contact Details

JBlumenthal


My Content

1 to 5 of 5 total
Posted By JBlumenthal Jul 10, 2026 04:09:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
My colleagues and I have discovered that if two of us open up the same Optix project that is located on a shared drive, the project does not open as read-only for whoever does not originally open it. This does not seem very safe for revision control. Is this a known issue?
Posted By JBlumenthal Jun 29, 2026 10:02:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am not able to find this Alarms Collection object within my project. But ultimately, you are saying there is no fix for this other than the application has to be restarted? There is no NetLogic that can be written to re-sync and re-initialize the object whenever the PLC does?
Posted By JBlumenthal Jun 25, 2026 03:58:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I am using the Alarm Widget from the Optix templates library to display tag-based alarms from a CompactLogix 5380 PLC. I have noticed that whenever I do a download of a program to the PLC, the alarms do not display/update until after I restart the application. Could this be an issue with the AlarmsEventLogger ...
Posted By JBlumenthal May 19, 2026 02:49:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I was wondering if it's possible for the Web Session of an application to access media files that are stored on an OptixPanel running the same application. I am playing video files stored on a USB drive plugged in to the OptixPanel. They display fine on the OptixPanel running the Native Presentation ...
Posted By JBlumenthal May 18, 2026 05:02:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I am using the Video Player UI object to play .MP4 videos from a USB drive that is plugged in to an OptixPanel Standard running the application. I have noticed a quirk when utilizing the Play and Pause event methods for the video player. If you pause and then play the video using these methods, the video ...