List of Contributions

Harding

Contact Details

Harding


My Content

1 to 6 of 6 total
Posted By Harding Sep 28, 2023 01:55:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I will try. I did try the different computer with no luck. I am trying not to wipe the entire drive so it will stay operational in between flash sessions... I will let you know how i make out. Thank you. ------------------------------ Harding --------------------------- ...
Posted By Harding Sep 28, 2023 12:36:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Sorry for the delay in response. I have struggled to connect to the drive using the USB route. It has a VERY slow response time. I was able to suck the parameters out of the drive, and when flashing the firmware I made it to 60% and it failed. The drive is still functioning and still gives ...
Posted By Harding Aug 31, 2023 06:47:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thank you for the reply. I have uploaded the log file for reference. I will also try the USB option as well. ------------------------------ Harding ------------------------------
Posted By Harding Aug 30, 2023 06:50:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I am trying to flash the firmware of a PowerFlex 525 from 5.001 to 7.001 without success. I am using ControlFlash 15.07 with Windows 11. I am able to see and pick the drive in ControlFlash, but it errors out at the end. The message I receive is "ERROR: Update to target device failed. Press View Log for ...