Posted By
Moser
Jun 02, 2026 03:16:00 AM
Found In
Egroup:
FactoryTalk Optix
\
view thread
Hello everyone, Optix Version: 1.6.1.15 Error description: The spinbox maximum value is linked to a control variable. This changes at runtime. For example, if the max is 10 and the Optix operator sets the spinbox to 10, then the control changes the max value to 5. The spinbox value remains at 10 and ...
|