List of Contributions

Ahmed

Contact Details

Ahmed


My Content

1 to 17 of 17 total
Posted By Ahmed Apr 08, 2024 04:05:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have imported an image from SYMBOL FACTORY (FT VIEW SE) and utilized it to develop screens in our OPTIX project. I would like add rotatory animation to my image and make it rotate in x-axis, but I couldn't find any references in FT OPTIX BASIC LAB, FT OPTIX ADVANCED LAB, or the Features Demo Project. ...
Posted By Ahmed Oct 06, 2023 07:11:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank You Shane for the information but why do I keep getting the below error as it doesnt allow me to compile. ------------------------------ Ahmed ------------------------------
Posted By Ahmed Oct 06, 2023 06:01:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I'm facing a security issue with user accounts and groups. I can't set a password for a user I've created, and even when I try, it's limited to just 4 characters. Additionally, I'm encountering an error when attempting to set a password. I would appreciate any guidance or references related to this problem. ...
Posted By Ahmed Aug 25, 2023 12:29:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello Daniel, I appreciate your clarification regarding the height information. However, I'm still facing uncertainty regarding the issue with the width, as I'm encountering difficulties fitting my objects within a constraint of 1520 units. Additionally, I'm unable to locate where I might have unintentionally ...
Posted By Ahmed Aug 24, 2023 11:59:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, I have already set FULL SCREEN to TRUE as you can see it from the screenshots I have shared. Still its not working ------------------------------ Ahmed ------------------------------
Posted By Ahmed Aug 23, 2023 12:11:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello y'all, hope you guys are doing okay. I'm using FT OPTIX Version 1.2.0.263 and I'm creating screens for my project. Im trying to create a panel in 1920x1080 resolution and I have added text and LED contents to it but when I'm running I run it on Emulator , the Panel doesn't fit properly on ...
Posted By Ahmed Aug 23, 2023 12:10:31 AM
Found In Library: FactoryTalk Optix
Posted By Ahmed Jun 08, 2023 11:24:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I would like to know what is the maximum storage capacity of FT OPTIX EMBEDDED DATABASE ? Also is the REPORT generated from the database customizable according to our requirements? If so can it only be done by writing QUERY or is there any other option? Would like to know more about how the ...
Posted By Ahmed Apr 12, 2023 01:24:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you for your reply, Im not sure I understand your statement, can you please elaborate ? ------------------------------ Ahmed ------------------------------
Posted By Ahmed Apr 11, 2023 11:40:00 PM
Found In Egroup: Automation Control
\ view thread
Hey Everyone, I am using MICRO 850E to communicate with Point IOs (1734-AENT, 1734-IB8(x6) , 1734-OB8(x4) , 1734-IE8C(x3)). Im able to successfully communicate all the modules with the Controller. The Digital Inputs and Digital Outputs (1734-IB8,OB8) are forced and verified BUT the analog inputs ...
Posted By Ahmed Mar 06, 2023 05:15:00 AM
Found In Egroup: Advanced Software
\ view thread
While creating a DISPLAY under HMI, I selected FactoryTalk View SE Display under PROCESS-5 and then I created a display. After assigning this display to all the compnenets in my ACM Project, I processded to generate display. While generating I got this error. I checked the location mentioned in ...
Posted By Ahmed Jan 04, 2023 04:16:13 AM
Found In Library: Automation Control
Posted By Ahmed Jan 04, 2023 04:16:00 AM
Found In Egroup: Automation Control
\ view thread
Hello y'all, I have a LC50-48QBB with me and Im trying to communicate it with a FLOWMETER FMF2040 via MODBUS RTU. I have used the MODBUS MSG block in CCW and Im not able to read any values from the flowmeter. can someone suggest me where I'm going wrong ? Also I'm getting an error '55' when I change ...
Posted By Ahmed Nov 15, 2022 09:36:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have a 1769-L32E controller attached with a devicenet module (1769-SDN) which consist of 7 nos of POWERFLEX40P Drive . How can I download the parameters of the drive without connecting my laptop to the drives? Is there a way I can download it through via ethernet cable from the controller? Or can I ...
Posted By Ahmed Nov 07, 2022 03:47:00 AM
Found In Egroup: Automation Control
\ view thread
I have a redundant control system which is working with L32E and Factory Talk View SE Version 6.0 (currently running in WINDOWS XP). Im able to ping my controller but when connected to my computer Im not able to access the CLIENT FILE and the data's are not showing up. Also while going through RS LINX ...
Posted By Ahmed Oct 28, 2022 11:24:00 PM
Found In Egroup: Automation Control
\ view thread
I have a Panel View Plus 1000 and its firmware version is 5.00.06.55. The PanelView is currently communicating with 1769-L32E which is obsolete so I'm planning to upgrade it to 1769-L30ER. So let me know if my PanelView Plus 1000 communicate or work with a 1769-L30ER? ------------------------------ ...