List of Contributions

Jozef

Contact Details

Jozef


My Content

1 to 17 of 17 total
Posted By Jozef Feb 22, 2012 12:34:00 AM
Found In Egroup: Automation Control
\ view thread
Summary: How to save bridged addresses? It is possible to configure 1756-ENBT as a bridge in RSLinx software for remote access to devices after the bridge card. But, if we configure 1756-ENBT card as an ethernet bridge the bridged IP addresses are not stored in the driver configuration. Therefore ...
Posted By Jozef Jul 23, 2011 03:54:00 AM
Found In Egroup: Advanced Software
\ view thread
One more question. Does everybody try to move screens from FTViewMe to RSView32? Is there any easy way to convert application from ME to RSView32? Jozef ##HL101
Posted By Jozef Nov 29, 2010 11:39:00 AM
Found In Egroup: Advanced Software
\ view thread
Thanks a lot. Do you ever know, is it similar situation for 5.0. Jozef ##HL101
Posted By Jozef Nov 27, 2010 08:16:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, I have a little bit different question. Is it any simple way to convert all ME application to SE? ##HL101
Posted By Jozef May 05, 2010 01:38:00 AM
Found In Egroup: Advanced Software
\ view thread
I have the same problem. Reinstallation RSView32 solve it. Jozef ##HL41
Posted By Jozef Apr 30, 2010 02:46:00 AM
Found In Egroup: Automation Control
\ view thread
As I know SLC does not support produced/consumed tags. But nevermind, this solution is rather complicate. Ihave finally get connection to RSLinx Gateway as Remote RSLinx Client, but I have to go back. When I configure RSView station connectes as Remote OPC Client to my RSSQL computer, RSSQL start ...
Posted By Jozef Apr 28, 2010 05:34:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Jonathan I am not sure if I understand you when you were talking about controller in the rack. Do you mean to use extra ControlLogix PLC (like 1756-L61) and make a data table for exchanging data between SLCs and PCs? But, then I have to make all the message communications between SLCs and ...
Posted By Jozef Apr 15, 2010 06:05:00 AM
Found In Egroup: Advanced Software
\ view thread
I am not sure what means "the tags are not there". I suggest to check the activity log and read all error messagese during application start. If you have development, you can look to tag database and try to check tag monitor. I also suggest to check node and driver settings. I wonder about lack ...
Posted By Jozef Apr 09, 2010 06:02:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I can give you some more info about ControlLogix Motion capacity. I have an application with 2x1756-L61 processors, 4x1756-M16SE and 2x1756-ENBT. Each processor use 2 SERCOS boards - one has 30 axis and the other 20 axis. All the Sercos boards work with Cycle Time 2 ms and CUP for 20 axis is set for ...
Posted By Jozef Apr 09, 2010 01:00:00 AM
Found In Library: Automation Control
Posted By Jozef Apr 09, 2010 01:00:00 AM
Found In Egroup: Automation Control
\ view thread
I had three separated lines, each one with two SCL 5/04 and RSView32 station for vizualization, recipe management and reporting (datalogging). At present, I need to connect these machines to LEVEL II system with Oracle database for Receipe and Reporting management which is using Transaction Manager for ...
Posted By Jozef Apr 07, 2010 04:40:00 AM
Found In Egroup: Advanced Software
\ view thread
I use such kind of communication with FTAC 2.31 and I have no problems. Are you sure you have the same RSLinx configuration in FTAC server and Adent(s)? ##HL41
Posted By Jozef Apr 07, 2010 03:35:00 AM
Found In Egroup: Advanced Software
\ view thread
You have to make 60 transactions. For distinction of each variables you can add aditional column with tag id. ##HL41
Posted By Jozef Apr 07, 2010 02:30:00 AM
Found In Egroup: Automation Control
\ view thread
I assume you log data using ODBC data source. Do you have enabled ODBC Backup Path and correct path in path window? Have noticed something logged to backup folder in the time where data stop to collect in SQL? Do you have any message in activity log in this time? ##HL41
Posted By Jozef Nov 13, 2009 12:27:00 AM
Found In Library: Automation Control
Posted By Jozef Nov 13, 2009 12:27:00 AM
Found In Egroup: Automation Control
\ view thread
I have attached a part of programm which makes a problem. You can download it to PLC to see how it works. ##HL38
Posted By Jozef Nov 11, 2009 11:47:00 PM
Found In Egroup: Automation Control
\ view thread
I have a program which uses the same 3 subroutines in sequence 3 times. The first subroutine has an input parameter which is a structure containing a few other structure, dint, int and bool (all together 20 bytes). Some of the structure elements are physical inputs of the PLC. For proper assigning of ...