Mohmad Sharif Tambrahalli
Contact Details
×
Enter Password
Enter Password
Confirm Password
Mohmad Sharif Tambrahalli
Profile
Connections
Contacts
Contributions
Summary
Achievements
List of Contributions
My Content
1 to 5 of 5 total
search criteria =
ALL
RE: Getting Active gateway status from Stratix 5700
Posted By
Mohmad Sharif Tambrahalli
Jan 25, 2024 12:59:37 AM
Found In
Egroup:
Networks
\
view thread
I might be wrong about the DLR faceplate. I will check this for sure and update this thread. Thanks A N
RE: Getting Active gateway status from Stratix 5700
Posted By
Mohmad Sharif Tambrahalli
Jan 25, 2024 12:48:44 AM
Found In
Egroup:
Networks
\
view thread
A N, Yes, i realised that the Redundant Gateway status is not displayed anywhere in the Stratix Faceplate including the newer versions. Because of the issue we faced with the v12.02 where the active switch faceplate was working, and the backup switch faceplate wasn't I got the impression that the AOI ...
RE: Getting Active gateway status from Stratix 5700
Posted By
Mohmad Sharif Tambrahalli
Jan 24, 2024 09:42:33 AM
Found In
Egroup:
Networks
\
view thread
DLR ports are in the same VLAN as CIP VLAN. With the older version of AOI, we are able to configure the path in the AOI itself without having to add the switch in the IO configuration tree. This was the only way we could make the faceplates work for both switches (configured as redundant gateway) ...
RE: Getting Active gateway status from Stratix 5700
Posted By
Mohmad Sharif Tambrahalli
Jan 24, 2024 09:11:13 AM
Found In
Egroup:
Networks
\
view thread
We are using the AOI and FT View ME faceplate. However, with version 12.02 of the library we faced issues. Backup gateway switch was always showing as unavailable in the IO tree. And the faceplate on the HMI didn't open. The faceplate for Active gateway switch was working fine and showing the correct ...
Getting Active gateway status from Stratix 5700
Posted By
Mohmad Sharif Tambrahalli
Jan 24, 2024 08:17:00 AM
Found In
Egroup:
Networks
\
view thread
Hi, In my project, we have configured a pair of Stratix 5700 switches as DLR redundant gateways. Is there any MSG instruction which can be programmed in ControlLogix to get the active/backup gateway status from the Stratix switches? Thanks in advance. ------------------------------ Mohmad Sharif ...
Copyright � 2024 Rockwell Automation. All rights reserved.
Powered by Higher Logic