List of Contributions

Arleybarc

Contact Details

Arleybarc


My Content

1 to 20 of 24 total
Posted By Arleybarc Feb 10, 2025 03:32:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello RA, I have some questions about Data Sources for an FT Optix Application. Is it possible to communicate with SLCs and Micro PLCs without using extra tokens (please see image attached)? Is it different to communicate with a Controller with an embedded Ethernet port than with an ENET Communication ...
Posted By Arleybarc Feb 10, 2025 03:31:30 PM
Found In Library: FactoryTalk Optix
Posted By Arleybarc Oct 23, 2024 08:57:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello All, I installed a Kinetix 5500 with an MPL-B330P-MJ74AA (Please see the image attached with the parameters trended). I want to perform the Out-of-Box Tuning recommended in the Motion System Tuning (at005) document, and in the end, the document highlights that may be required to reduce the ...
Posted By Arleybarc Jul 24, 2024 09:20:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Vincent, We need to get the risk assessment first. Also, I appreciate your comments for future reference. Thank you for your time. Have a good day. Arley
Posted By Arleybarc Jul 23, 2024 07:25:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Vincent, I want to protect both humans and equipment, but mainly humans. This door opens and closes horizontally on a powder paint booth; therefore, the pollution is high. What kind of servo drive could be configured to auto-reverse (like a garage door)? Sincerely, Arley
Posted By Arleybarc Jul 22, 2024 11:09:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello All, Is it possible configure a Kinetix 5500 to auto-reverse as a safety feature? or Do you know a reliable method to programm a Servo Drive for auto-reverse? I am looking forward to your comments. Have a good day. Sincerely, Arley
Posted By Arleybarc Jun 20, 2024 03:18:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Vincent, The Actual motor Tuning parameter and inertia setting on the Kinetix 350 are the default ones. General: - Axis Configuration: Position Loop - feedback Configuration: Motor Feedback - Application Type: Basic - Loop Response: Medium Scaling: - Units: Position Units - ...
Posted By Arleybarc Jun 19, 2024 10:34:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Vincent, Thank you for sharing these documents. The load is a Booth Door (Closed-loop servo system application). The Servo Motor (MPL-B330P-MJ74AA) opens and closes the door (Open: MAM / Position -88) to (Close: MAM / Position 0). The challenge is that the routine that governs the door's operation ...
Posted By Arleybarc Jun 18, 2024 12:14:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Performing the Kinetix 350 to Kinetix 5500 migration on Studio 5000 Logix Designer, when I add the new Module (2198-H025-ERS) and update the existing Axis, under axis Properties / Categories, there are some differences as expected. However, in particular, the properties listed below change the default ...
Posted By Arleybarc Jun 14, 2024 03:22:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Vincent, Thank you for your response. Yes, we should be fine. This question is kind of obvious, but to be sure, I will ask you. The former K350 had wired STO pinouts #4, 5, and 6. Could the new K5500 be wired to the S1, SC, and S2, respectively?
Posted By Arleybarc Jun 11, 2024 08:42:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Yes, they had replaced fuses a few times before. The problems with the K350 were multiple. ENET communication was intermittent; also, the Servo Drive was faulted (indicators M and A were red); then, after rebooting, M and A flashed green without any code. After checking the installation, I noticed ...
Posted By Arleybarc May 13, 2024 11:48:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Batman, Thank you for your response. I will select the Kinetix 5500 (2198-H025-ERS) using an MPL-B330P-MJ74AA. In our application, teammates told me that they were forced to replace fuses on the AC Power several times before the Kinetix 350 failed. Could you please tell me more about the criteria selection ...
Posted By Arleybarc May 03, 2024 09:17:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I am ready to replace a Kinetix 350 with a new Kinetix 5300. I wonder what is the best practice on Studio 5000. Should I create a new axis and move the existing one to Ungrouped Axes folder? should I create a new tags instead of reuse the existing ones? Any comments and recommendations are welcome. ...
Posted By Arleybarc Apr 29, 2024 09:56:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Vincent, I do not have the motor fixed on any surface, I am working on a workstation. I am configuring a Kinetix 5300 Servo Drive: 2198-C4020-ERS, and a Servo Motor: MPL-B330P-MJ74AA.
Posted By Arleybarc Apr 29, 2024 08:06:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Vincent, I am replacing the Servo drive K350 to K5300. The motor does not have the load attached. I am using the default values: Position Units, 1.0 Position Units per 1.0 Motor Rev.
Posted By Arleybarc Apr 29, 2024 07:40:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, Batman. Thank you for your response. I replaced the motor, and the fault is no longer present. However, are there configuration parameters to consider to avoid this fault? I am working on the training lab with a brand new K5300 and used MPL Servo Motors. Testing the motion direct commands, MAJ-Speed ...
Posted By Arleybarc Apr 26, 2024 11:27:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I just got this F11 Fault working with a Kinetix 5300. What does the fault F11 means? Any idea what to do?
Posted By Arleybarc Feb 26, 2024 07:42:00 AM
Found In Egroup: Advanced Software
\ view thread
GLaDOS, Thank you for describing the different options for this particular alarm application. I like the concept behind the logic to control the alarm behavior in the controller and govern Digital bits for alarming. However, I am also tempted to use the FTAE features. Therefore, I will combine both ...
Posted By Arleybarc Feb 23, 2024 08:42:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello All, I need to configure an alarm to track a pressure value; therefore, I will configure a Deviation Alarm. However, the process finishes on Friday night and starts on Monday morning. How can I avoid triggering the alarm when the process stops, even though the pressure drops drastically to zer ...