List of Contributions

Ron

Contact Details

Ron


My Content

1 to 20 of 50+ total
Posted By Ron Feb 07, 2025 08:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
It turns out it was a firmware isue. The version I was using had a memory leak. I haven't tested the new firmware but I heard from a customer that the new firmware fixed the issue.
Posted By Ron Dec 10, 2024 02:19:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I understand. I can implement that widget. Thats a good tip. But this isn't possible anymore when the FT Optix application is crashed. Is there another way to get there with a web browser or something? I got this screenshot from someone but couldn't figure out how to get there.
Posted By Ron Dec 10, 2024 02:18:57 AM
Found In Library: FactoryTalk Optix
Posted By Ron Dec 10, 2024 01:09:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
The FT optix panel still crashes after 3 days. So deleting the set time script didn't work. Is there an easy way to check the process memory? Maybe we can see that this is filling up and not wait for 3 days until the crash. That takes a lot of testing time. With kind regards, Ron
Posted By Ron Dec 06, 2024 03:05:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I'll take out the set time logic and check if the crash is still there. The warning shouldn't be the problem. It only stops creating the HMI objects. But still that doesn't explain why the HMI doesnt crash after a 4 hours anymore but after 4 days when deleting the loggers.
Posted By Ron Dec 06, 2024 01:46:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello all, I've got a question about the FT optix runtime. The project I made randomly crashes. After that it is only giving a black screen. when I do a power cycle, the optix runtime application starts again. At first it crashed after 4 hours. I deleted all loggers that loggers that are ...
Posted By Ron Dec 06, 2024 01:45:40 AM
Found In Library: FactoryTalk Optix
Posted By Ron Oct 23, 2024 05:12:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I had a PLC project where I deleted a bunch of stuff because it was causing overhead. When importing I deselected al these tags. After that it gave this error. Eventually I figured out what the problem was by deleting all the datatypes by hand. It turns out that some of the tags were ...
Posted By Ron Oct 21, 2024 07:00:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello all, I'm searching for a fix for the following error when trying to edit the tag import. When deselecting some of the imported tags that are not available anymore it gives the following error. And doesn't import the tags. Category: TaskConsumer Message: Exeption caught: Data type ...
Posted By Ron Oct 04, 2024 08:16:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello all, For a project I need to have a retentive data for at least 2500 tags. I want to make a "Retentivity storage" where I add all those tags. I was hoping that there was an import/export script available just like for the alarms or key converters but couldn't find any? Is there a fast way ...
Posted By Ron Jun 19, 2024 07:29:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello all, I've got an FT Optix C# coding question. I want to read out a value of a tag. But this tag is never used in the HMI. The code that I'm using right now is the following: Project.Current.GetVariable(path3+"/Parameters/GenerationNumber/iValue").Value; This value reads out "0" when ...
Posted By Ron Jun 06, 2024 02:44:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello all, I've got an FT Optix screen that is quite small. its only 7 inches. Therefore, the keyboard that's on screen is also small. This keyboard is not filling up the total width of the screen. Is it possible to resize the on-screen keyboard so it will be easier to handle for an operator? ...
Posted By Ron May 16, 2024 01:12:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for the quick response. The line I see is acceptable. I saw this line and wanted to know what it was. And because I saw it, I also wanted to point it out for people with the same problem. It also happens in version 1.4.0.884-ReleaseCandidate. And on the physical runtime on the HMI.
Posted By Ron May 15, 2024 08:51:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello all, I have a problem with the spinbox object. When I change the border color from the default button in the stylesheet, it shows a weird line in the spinbox buttons. The only thing i changes was the border color of the default button style. The line position also ...
Posted By Ron Mar 26, 2024 03:16:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
It turns out I'm still using an old script that I took out the library in optix version 1.2. That's why the export didn't work. With the new script I'm able to export the alarm. Now I hope my own excel alarm generator still works with this new script. But that's another issue. Thanks for the in ...
Posted By Ron Mar 22, 2024 08:34:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I kind of tried it this way. But when trying to export or import the alarms it doesn't take the variables with it. So I'm a little afraid when I do it this way I will get problems with importing and exporting alarms. At this moment I made some Key converters that looks at the alarm name in optix. So ...
Posted By Ron Mar 13, 2024 10:21:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello all, I have a question about some data management and don't really know the best way to implement this in FactoryTalk Optix. I want to automatically open a popup when an alarm is generated. This popup will show 3 to 5 different causes that could have triggered this alarm. There will also ...
Posted By Ron Feb 28, 2024 12:47:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I also called Rockwell and made a ticket. They said its already in the list of R&D and they say it should be fixed in V1.4. So I guess I'll have to wait till then,
Posted By Ron Feb 26, 2024 02:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello @Delete, It looks like the recipe schema gives the problem. When I deselect all the tags in there and try to import my PLC tags, it works. With kind regards, Ron
Posted By Ron Feb 15, 2024 12:54:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I tried deleting the comm driver. But after saving optix was shutting down. The same was happening when trying to delete the maps inside. Copying the files from the new project to the existing caused an optix crash as well. I already made a ticket as soon as I had this problem but ...