List of Contributions

Janacek

Contact Details

Janacek


My Content

1 to 4 of 4 total
Posted By Janacek Sep 04, 2025 04:49:00 AM
Found In Egroup: Automation Control
\ view thread
We flashed the panel several times. We tried versions from 12 to the latest 15.1, which we have now. We are sure that the IP address and network mask are correct. RSLinx Classic sees the panel and communicates with the PLC, but FTLinx does not see it. We managed to track down the following ...
Posted By Janacek Sep 02, 2025 09:40:00 AM
Found In Egroup: Automation Control
\ view thread
Hi DPer. Yes, I tried it. The PVP did not appear as a new USB device connected to the PC. Therefore, it was not visible in FTLinx under the USB driver. Thank you for your reaction.
Posted By Janacek Sep 01, 2025 01:00:00 AM
Found In Egroup: Automation Control
\ view thread
Hello. We are using the new PanelView Plus 7 Performance 1200W and are having connection issues. I can't see it in FTLinx. When I add it manually, it has a red cross. It is not possible to upload or download the runtime application. RSLinx Classic sees it normally. We tried firmware and studio versions ...
Posted By Janacek Aug 28, 2025 09:16:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello. Did you manage to solve the problem with FTLinx in the end? I tried all the suggestions in this thread, but nothing helped. I still can't see the HMI... -------------------------------------------