List of Contributions

MERRILL

Contact Details

MERRILL


My Content

1 to 20 of 38 total
Posted By MERRILL Mar 09, 2026 12:45:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
We have used Factory Talk Optix as a SCADA Solution running it on a virtual server. We had the customer upgrade this virtual server from 64GB to 256 GB RAM to ensure the project loads and operates correctly. This is also a Heavy project with around 200,000 alarms and roughly 6 million nodes. The project ...
Posted By MERRILL Jul 16, 2025 08:02:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
My apologies please see the attached project.
Posted By MERRILL Jul 15, 2025 03:20:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I didnt explain this correctly in the last message on how to achieve this. Thank you for your example project. I have modified the project with a working example of a combo box to toggle different data loggers. The data loggers are just connected to model variables that are being saved in an embedded ...
Posted By MERRILL Jul 14, 2025 01:38:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
What I usually do for this is create a combo box on a page with a panel loader below the combo box. Also put the panel loader into a scroll view then, i point the panel loader to the selected item of the combo box, then point the combo box model to a folder that is a collection of the Advanced Trend ...
Posted By MERRILL May 09, 2025 02:43:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
can you try setting the cool down for 1 second? or it also looks like the GITHUB has an updated project as well. https://github.com/FactoryTalk-Optix/Optix_Sample_SMSDispatcherGSMSerial Let me know if you still need help with this
Posted By MERRILL Apr 30, 2025 09:42:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Nothing should be saved as secrets so you should be okay.
Posted By MERRILL Apr 30, 2025 08:30:00 AM
Found In Library: FactoryTalk Optix
Posted By MERRILL Apr 30, 2025 08:30:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
It wont let me upload a z file so i tried zipping it but it may not work out let me know if you cant get the project open after you extract it. sometimes it works for me and sometimes it has errors.
Posted By MERRILL Apr 30, 2025 07:19:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Here is the one that I used and have got to work on a live system. I used a MultiTech Modem for the Serial Connection. Take a look at the attached z file and let me know if you hae any quesitons.
Posted By MERRILL Apr 30, 2025 06:15:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have a working sample project i can upload for you on this. Give me a day or two to take out names and numbers and ill upload it for you!
Posted By MERRILL Feb 21, 2025 03:29:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
The serial port name for the device i matched to the coms driver in the device manager which is COM3, I got it to were i can open the port but I get no response from the cell modem. I tried hovering over the error message but i cant get it to show where the issue is in the code. Ive definatly had ...
Posted By MERRILL Feb 21, 2025 11:57:17 AM
Found In Library: FactoryTalk Optix
Posted By MERRILL Feb 21, 2025 11:57:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am trying to get the SMS Dispatcher GSM Serial application from the github to work with a seirra wireless RV 50 cell modem. I cannot get the Optix application to connect to the serial port of the modem as well im getting a fault saying the following has anyone gotten this to work or tried it before? ...
Posted By MERRILL Feb 21, 2025 09:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have tried this but was unable to get it to work when i tested it.
Posted By MERRILL Jan 28, 2025 07:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
This worked thank you!
Posted By MERRILL Jan 27, 2025 04:34:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Im working on deploying a new FT OPTIX RUNTIME and I am getting the following errors / Warnings / Messages. The runtime states its only using 6 feature tokens and im licensed for 11. I also get a warning saying the project requires an unlimited entitlement. 2025-01-27 14:11:45.169;urn:FTO ...
Posted By MERRILL Jan 16, 2025 10:37:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
This works Thank you! I didnt think about this.
Posted By MERRILL Jan 16, 2025 07:58:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Sorry here is the file