List of Contributions

Michael Harris

Contact Details

Michael Harris


My Content

1 to 11 of 11 total
Posted By Michael Harris Mar 03, 2026 06:19:02 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Campbell, The database files are not included in the AOP download. They are a separate download. You have 2 options for obtaining the database files. Option 1: Connect to the drive using CCW with the PC you are trying to do the conversion on. CCW will upload the database file from the drive and store ...
Posted By Michael Harris Feb 21, 2026 10:32:52 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello Austin, Both Vincent and Batman are correct but I wanted to provide a little more context. Option 2 (MGSP) is good when the axes are at rest or if you are not trying to obtain the position for a specific instant in time (like a registration event). When an axis is moving, you will not ...
Posted By Michael Harris Sep 23, 2025 11:57:06 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
How do you have A558 [Positioning Mode] configured? If set to 2 "Step Logic" it will always start at Step 0. To get the functionality you are looking for, it must be set to option 3 "Preset StpL" See below" I hope this helps-------------------------------------------
Posted By Michael Harris Jul 31, 2025 06:56:00 AM
Found In Egroup: Automation Control
\ view thread
I apologize if you are already aware of the information I am sharing but it threw me the first time I encountered it. DMK files are compatible with both ControlFLASH and ControlFLASH Plus. For Logix controllers V30 and below, the inventory groups the firmware by Controller part number. You will notice ...
Posted By Michael Harris Oct 11, 2023 07:24:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Luke, I do not know where this is documented but Soft Overtravels are an "Absolute" function and typically absolute functions require homing. I believe Vincent is correct that you will need to home the axis to get Soft Overtravels to function. This does not mean you need to abandon ...
Posted By Michael Harris May 23, 2023 07:17:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
pa_servo_guy I agree with Vincent. The behavior you described is usually an indication of an internal drive failure and you should work with your local representative. If you would still like to try flashing the drive, I may be able to help with that. Newer firmware has a security feature called ...
Posted By Michael Harris Sep 01, 2022 10:53:00 AM
Found In Egroup: Automation Control
\ view thread
Correct. You have the current only version .5-30A ------------------------------ Michael Harris ------------------------------
Posted By Michael Harris Aug 31, 2022 01:04:00 AM
Found In Egroup: Automation Control
\ view thread
Ryan, There are three varieties of sensing module. They are Current, Current/Gnd. Fault. and Current/Gnd. Fault/Voltage. To get kWhs, you need to have the latter. Please verify which sensing module you have. ------------------------------ Michael Harris ------------------------------
Posted By Michael Harris May 20, 2022 12:38:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
The cmf file does not just contain motor information. It also specifies which drive products the motor is compatible with. If you received the cmf file prior to the K5300 being released, the K5300 would not be specified in the file and therefor the motor would not appear in the drop down list for that ...
Posted By Michael Harris Apr 08, 2022 01:43:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I do not know if this has been implemented on the K5300, but would expect not. As pointed out, demo mode was used to operated the 460V 3phase drive on 230V single phase in a classroom or hands on lab environment (demonstration). It is not suitable for production environments. Since the K5300 is available ...
Posted By Michael Harris Dec 21, 2021 03:20:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
There are no program modifications required. The new drive has hardwired STO only so all the additional functionality is achieved with wiring only. If you do not want to use STO, use the jumper supplied with the drive and it will operate the same as the original. ------------------------------ Michael ...