Posted By
Hogan
Aug 13, 2026 08:24:55 AM
Found In
Egroup:
Automation Control
\
view thread
Usually, when the output ramps up continuously to maximum and never drops during autotune, it means one of three things: Incorrect Control Action (Direct vs. Reverse): If the loop is set to Direct acting when it should be Reverse (or vice versa), the controller will drive the output in the wrong ...
|