I created a project to collect the parameter files on our PF525 & PF753 drives. Having an issue with CCW v20.01.00 crashing about half of the time when I add a new device. It deletes the recently added device, appears to close CCW, then re-opens. I'm using the "select existing device" then browsing ...
|