List of Contributions

aOptixUser

Contact Details

aOptixUser


My Content

1 to 20 of 24 total
Posted By aOptixUser Oct 13, 2026 02:26:27 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Have you added any graphical elements to Window_1? I often do that to see the difference between the two window types. To me, it looks like you are using an blank Window_1 without any graphical elements.
Posted By aOptixUser Oct 12, 2026 01:21:17 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Correct :) So i have done this in the example project
Posted By aOptixUser Oct 12, 2026 12:45:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey, I think you're jumping the gun a bit here. If I understand correctly, you want to display specific content on a screen. http:// /windows/Dashboard/windows/Dashboard This link doesn't access panels within the Optix Runtime; instead, it accesses specific containers of the "Window" type. Solution: ...
Posted By aOptixUser Oct 08, 2026 07:57:15 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey MJ, On GitHub you can find some example projects - I found this one there. It contains an example of how to solve your problem. I've tested it, and the same web engine shows me two different screens depending on the URL. Optix_Sample_WebPresentationEngineSessions Maybe you can find some helpfull ...
Posted By aOptixUser Sep 24, 2026 12:55:45 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Vinoth, If you really need a reload function, you can create a Boolean tag for toggling in the session or model and add a "ChangedEvent" to it. With this event, you can trigger the "ChangePanel" method on the required panel loader. You can add the same panel as before as the new panel, and the ...
Posted By aOptixUser Sep 08, 2026 12:52:51 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey, sorry for the late reply. I was oon vacation and couldn´t look into the issue afterwards because I was needed elsewhere. I am tho owner of the repository, so the URL hasn´t changed. Unfortunatley, I still can´t connect to the repository. Apologies again for the late reply. - ...
Posted By aOptixUser Jul 31, 2026 01:28:23 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Many thanks you saved my day :)
Posted By aOptixUser Jul 30, 2026 09:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, dear community, the image below shows how we defined TagBasedAlarms in a project. How can I read or evaluate the AssociatedTags in Optix at runtime? We want to use this tag to implement FirstFaultDetection, which worked up until Optix version 1.7. Unfortunately, I can no longer find a ...
Posted By aOptixUser Jul 07, 2026 06:29:31 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Okay, I tried again. This time, I'm getting the following log message. But I don't understand this message, and I can't find any documentation about it either.
Posted By aOptixUser Jul 06, 2026 11:59:47 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Sorry for my late reply, i would try it. Thanks for helping ^^
Posted By aOptixUser Jul 02, 2026 03:28:50 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for the quick reply :) We tried again, but the result is still the same. Optix Studio shows that the provider is unavailable. We also tried using different URLs, but the result is always the same. So, when we followed the instructions from Bitbucket and entered the URL shown in the image ...
Posted By aOptixUser Jul 02, 2026 01:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, everyone. I have a question about version control using the cloud version of Bitbucket. We'd like to manage the project using Bitbucket as a cloud solution. However, in the settings, we can only find the on-premises option. Is there a workaround that would allow us to use Bitbucket (Cloud) ...
Posted By aOptixUser May 19, 2026 12:14:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Gerdes, I'm not sure if this matches your problem, but we once had a similar issue in our project. Do you have NodePointers or aliases with a specified child on the objects you want to copy? If so, this can also cause problems because the types specified on the child are copied along with ...
Posted By aOptixUser May 07, 2026 12:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Paul, did you add the X button yourself, or are you referring to the X button in the runtime window? If you added the X button yourself to close the runtime, you can use a so-called Formatted Dynamic Link to control the button's visibility property. With this, you can target specific user ...
Posted By aOptixUser Apr 22, 2026 12:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Retzlaff, Do you only want to display this number? If you only want to display this number, you can do so using an ExpressionEvaluator: Expression: "(PLC_Value)/100". Alternatively, you can cast your integer to a float using an ExpressionEvaluator: Expression: "(float)PLC_Value". ...
Posted By aOptixUser Apr 10, 2026 05:05:00 AM
Found In Egroup: Advanced Software
\ view thread
Hey Wrage, welcome here :) Which container do you use ? In case you are using the AlarmHistoryGrid from the Library, there is an "Auto refresh time" - property. Id the value is 0 the automatically updating is disabled. -------------------------------------------
Posted By aOptixUser Mar 03, 2026 12:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi @Flareux, I had the same problem in the same scenario. I solved it by registering an event observer that reacts to a UserLogout event and then terminates the current workflow with a method invocation. It's important that the method call isn't implemented on the dialog box itself. Otherwise, ...
Posted By aOptixUser Jan 15, 2026 07:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello Community, I have the following problem: The customer sometimes wants a four-eyes principle (dual acknowledgement) for his alarms. The workflow looks like this, Any employee can acknowledge alarms if they are logged in, but only an employee with a higher user level can confirm ...
Posted By aOptixUser Jan 13, 2026 01:10:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, First things first, happy new year :D. Sorry to reply so late. I was just about to write the answer, with screenshots of course. I noticed an error in the flow of the methods. Here the problem was that the dialog box was closed and only then the cancel method was executed - ...
Posted By aOptixUser Dec 22, 2025 02:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello everyone I have the following problem: I have to use SignWorflow for the alerting (4-eyes principle), the user who confirms the alarm has to authenticate. I solved the problem like this: The definition of the alarm takes place in the model, from which the instances for the actual alarming are then ...