List of Contributions

Tomasino83

Contact Details

Tomasino83


My Content

1 to 18 of 18 total
Posted By Tomasino83 Mar 20, 2026 05:28:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
This is the error on the browser console -------------------------------------------
Posted By Tomasino83 Mar 20, 2026 05:14:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Is Chromium version 89 supported? I get the same blank screen with this browser. -------------------------------------------
Posted By Tomasino83 Dec 12, 2025 01:59:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I think you need to use an expression evaluator, like that: -------------------------------------------
Posted By Tomasino83 Dec 01, 2025 09:25:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Changelog for 1.6.5.1 seems truncated, where can we find a good one? -------------------------------------------
Posted By Tomasino83 Nov 27, 2025 01:55:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Dynamic polling time should be configured also for alarm configuration (property of project), not only for NativePresentationEngine. Have you tried changing that value? Please share performance result with alarm bits grouped in DWords, it seemes an interesting solution! BR ...
Posted By Tomasino83 Oct 21, 2025 12:02:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you all for your replies. Your point about undocumented methods is clear and makes absolutely sense. Anyway, since there is a "cheat sheet" with snippet codes that can be useful, I'm trying to underdstand how to make them working: hopefully, someone looking at this forum has the answer. Forget ...
Posted By Tomasino83 Oct 21, 2025 06:17:25 AM
Found In Library: FactoryTalk Optix
Posted By Tomasino83 Oct 21, 2025 06:17:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I want to create dynamic Link in NetLogic because I don't know how to manage different dynamic link based on the datatype. E.G., sometimes I need to write a string or a LocalizedText on a Label depending on a boolean, but runtime will give me a warning for mixed datatype. Another example, I may want ...
Posted By Tomasino83 Oct 20, 2025 11:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I've tried to add an advanced dynamic link for the Text property of a Label as explained in NetLogic_CheatSheet, I added the code in the start method of a NetLogic in the same widget (Type) of the Label. I made a lot of unsuccessfull attemps (Text was stuck to original static value), until ...
Posted By Tomasino83 Sep 08, 2025 02:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
You have a lot of workload indeed! Some thoughts. You wrote about several application crashes: rarely an high CPU load causes process to crash, it usually just make things slow or unusable. Try to investigate which application is crashing (optix or dataacquisition) and (more difficult) why. Optix ...
Posted By Tomasino83 Sep 08, 2025 01:51:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
In theory you can leverage the project's OPC UA architecture to build a client/server project like in this sample: FactoryTalk-Optix/FeaturesDemo2_M2M_Client: OPC/UA synchronization of screens, tags and alarms But in practice you should check very carefully if you can still manage in a consistent ...
Posted By Tomasino83 Sep 02, 2025 03:40:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I can't find an executable DataAcquisitionCore.exe in my optix installation. Try to find the file location to make sure it's related to Optix. Bad CPU performance on VM could be also an issue on the HOST where you are running the VM. Adding more core to the VM could also lead to worst performance ...
Posted By Tomasino83 Mar 13, 2025 03:25:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
AFAIK optix panel only support LDAP, not activeDirectory. Try a configuration like this: CA certificate is also needed. Replace "testdc" with the hostname of the domain controller. Make sure you can ping "testdc.test.local" from the diagnotstic page of the panel.
Posted By Tomasino83 Feb 13, 2025 01:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Another option without using a logger could be to observe alarm events as in this sample code: Subscribe to new alarms and get notified at every Acknowledge or Confirm event I don't know if there's a variable tracking how much time an alarm was on, probably you need some extra code to record ...
Posted By Tomasino83 Jan 28, 2025 08:44:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Unfortunately for some reason ViewModel children count doesn't get updated when rows get removed! So you see the counter being updated each time you hit a new maximum, but it never decreases. I've attached code that observe reference add/remove, remove event never gets fired. Same behaviour ...
Posted By Tomasino83 Jan 28, 2025 08:43:37 AM
Found In Library: FactoryTalk Optix
Posted By Tomasino83 Jan 28, 2025 03:42:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Good catch AutomateSHANE! I tested your code against an alarm grid, it returned the number of alarm displayed. I can't see ViewModel from UAExpert, but from the VS debbugger it seems ViewModel and its children are all UAnodes: maybe you can register as event observer on the Children node of ViewModel ...
Posted By Tomasino83 Nov 19, 2024 02:00:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I think/hope it will be possible since relese 1.6, currently in beta: