List of Contributions

oliveira

Contact Details

oliveira


My Content

1 to 7 of 7 total
Posted By oliveira Oct 16, 2022 05:07:00 PM
Found In Egroup: Automation Control
\ view thread
Yes, it worked! I left it with the same values and it worked perfectly, now I just need to make one more HSC work. thank you very much for the support ------------------------------ oliveira ------------------------------
Posted By oliveira Oct 14, 2022 08:51:00 PM
Found In Egroup: Automation Control
\ view thread
------------------------------ oliveira ------------------------------
Posted By oliveira Oct 12, 2022 05:59:00 PM
Found In Egroup: Automation Control
\ view thread
but... but the second counter goes into fault number 4 ------------------------------ oliveira ------------------------------
Posted By oliveira Oct 12, 2022 05:58:30 PM
Found In Library: Automation Control
Posted By oliveira Oct 12, 2022 05:54:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, the primary counter has these settings and works perfectly.
Posted By oliveira Oct 08, 2022 05:03:00 PM
Found In Egroup: Automation Control
\ view thread
OK, but then if you want to use inputs 0 and 1 in the first counter and inputs 2 and 3 in the second counter, what would the instructions and their HscID look like? ------------------------------ oliveira ------------------------------
Posted By oliveira Oct 07, 2022 09:38:00 PM
Found In Egroup: Automation Control
\ view thread
Guys, I'm having difficulties using two fast counters (HSC), I would like to know which values are suitable for the HscID variable, because in the first counter I programmed I put a value of zero (0) and in the second I don't know which value to put and the same is not works correctly. I wait for subjects. ...