List of Contributions

pmkg

Contact Details

pmkg


My Content

1 to 20 of 29 total
Posted By pmkg Jul 31, 2025 11:39:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have found current limit value low. So after change that value it works fine. -------------------------------------------
Posted By pmkg May 05, 2025 07:09:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I have issue with one of the armor power flex 35s drive. When I give Forward Direction + Start command then the actual command also same Forward. Then stop and start again with reverse direction command, but driving actual direction still same Forward Direction. Then stop one more ...
Posted By pmkg Mar 20, 2025 09:25:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi , What is the value velocity output in armor power flex. What Is relation to Frequency? Thanks
Posted By pmkg May 02, 2024 03:28:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi everyone, I facing issue with armorstart 281e. When run command forward , getting running forward feedback. But when I run reverse not getting running reverse feedback. Sometime it's coming. See the video attached. It's shows Run indication but physically not happening. ...
Posted By pmkg Mar 25, 2024 06:42:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi fuzz, Thanks for reply, it is confusing when you check same manner AccelRedSelect_0 to AccelRefSelect_2. And the velocityRefSelect_0 to VelocityRefselect_2 On page 176 table and page 201 data somewhat mismatch. Thanks
Posted By pmkg Mar 23, 2024 08:00:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Everyone, I need clarification on DirectionCommand_0 & DirectionCommand_1. As per manual , DirectionCmd_1 = ON & DirectionCmd_0 = OFF for Forward direction running. But it actually reversed. When DirectionCmd_0 = ON & DirectionCmd_1 = OFF running Forward direction. ...
Posted By pmkg Mar 22, 2024 08:07:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Fuzzy, I have studio 5000 V35.0 AOP version 1.2.51 Drive configured as Standard and Safety. While doing auto tune I plugged hardware STO and Ownership reset to make out of box. It went to hardware safety STO. The I started Tuning static and rotate tuning both ...
Posted By pmkg Mar 21, 2024 09:34:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Fuzzy logic, I did the same way. Auto tune happening but I could not save the tuned values. Accept test value and then finish press getting AOP apply error
Posted By pmkg Feb 26, 2024 07:32:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Mendoza, Change the drive parameter to add datalinks, Datalink A1 Added, Then link the Output current to Datalink A1 Then update DeviceNet IO Input Length to match how many datalink added based on. You will get the data in PLC
Posted By pmkg Feb 26, 2024 07:15:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
fuzzy logic, Thanks for reply, it is network safety armor power flex. i have more than 50 devices. is really required to changed connect standard only ?
Posted By pmkg Feb 23, 2024 12:20:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Dear all, I read out the manual , it says "Autotune cannot be performed" when a safety connection has been configured. I have 50 armor power flex drives configured to PLC project. all are configured with Standard & safety. is really tunning required when using conveyors? ...
Posted By pmkg Feb 23, 2024 12:16:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Mendoza, this may help if are using ENET communication, Add what data want read from drive. once completed it will reflect in Input tag member Thanks,
Posted By pmkg Feb 10, 2024 04:05:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Everyone, I commissioned two projects with TYPE J Thermocouple. below the configuration window. My problem is physically measured temperature and Module Read value is not matching. There is more difference. So i have to use cold junction offset to match the read value ...
Posted By pmkg Feb 05, 2024 05:43:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi everyone, I configured Powerflex 755 with DeviceNet Communication. Like this i am starting and stopping. Start & Stop functions are found Good. But problem is Drive Ready (Status bit 0) getting transition High to Low then Low High within 1 sec. This is happening every cycle. ...
Posted By pmkg Jan 25, 2024 08:26:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Could you explain what is the values are used in SCP.
Posted By pmkg Jan 04, 2024 10:30:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
UDT Tag is DINT For that UDT i am moving Values in REAL data type. UDT Moving to Scanner DINT address. ------------------------------ pmkg ------------------------------
Posted By pmkg Jan 04, 2024 09:09:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I checked parameter 1 & 2 . It almost 0. So that I checked which port we give ln reference to 545. 545 reference given from 874 ( Port 4 reference). There itself it's not coming anything. If change to HIM reference Port 2 values are updating . That's shows in picture ...
Posted By pmkg Jan 04, 2024 07:56:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Daniel, Thanks for your clear explanations. I did the same steps. but i have problem port reference itself. I connected the DeviceNet card in Port 4. i am getting Logic commands but not speed reference. Can we send 60 Hz in PLC 60 value? or any multiplications ...
Posted By pmkg Jan 01, 2024 04:44:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Everyone, I have problem with PowerFlex 755. I configured DeviceNet card to L73 DeviceNet Scanner. Logic status , additional Data links getting in PLC side. Logic command and additional Data links moving to Drive side. Only problem with speed reference Its moved to DeviceNet Scanner ...