List of Contributions

Haldar

Contact Details

Haldar


My Content

1 to 20 of 50+ total
Posted By Haldar Jul 14, 2026 11:43:11 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Luca, Thank you for the information. I have observed that this issue occurs when the client or user double-clicks the runtime.exe icon while the application is already running. In this scenario, the application should not close. Instead, it should display a message indicating that the application ...
Posted By Haldar Jul 14, 2026 03:47:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi All, Below error logged in file. what is the meaning of that ? 4-07-2026 12:14:15.279;ERROR;FTOptixRuntime;210003d;Exception caught: Unable to create ObjectType table - error message: database is locked;stack dump [0] Core::Token::JWTToken::ToString stack dump [1] Core::Token::JWTToken::ToString ...
Posted By Haldar Jul 10, 2026 10:22:42 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Luca, Thats the point which i asked that why orange icon for runtime application ? because in other projects , i saw blue icon only. ------------------------------ Soumen ------------------------------
Posted By Haldar Jul 09, 2026 11:12:48 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Noah, I have checked already log file in which demo statement is not showing. Its showing how many entitlements are present. ------------------------------ Soumen ------------------------------
Posted By Haldar Jul 09, 2026 10:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Team, In one of our projects, as shown in the screenshot below, the icon is displayed in orange instead of blue. We observed that in other projects, the icon changes from orange to blue after activation, even though the runtime is started from the emulator or the Runtime Application folder. We ...
Posted By Haldar Jul 07, 2026 07:03:40 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Baic, After looking the same KB note only , i contacted Engage Team for support. ------------------------------ Soumen ------------------------------
Posted By Haldar Jul 06, 2026 05:18:31 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Luca, Noted I will inform to client accordingly but during rehosting , confirmation window is not coming with yes/no which is somewhat strange to me as i tested in one of office system. ------------------------------ Soumen ------------------------------
Posted By Haldar Jul 06, 2026 03:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Team, Customer asking for steps by steps for transferring Entitlement Key from 1st PC to 2nd PC but Internet connectivity is not available in both PC. Please provide the document or link ------------------------------ Soumen ------------------------------
Posted By Haldar May 19, 2026 09:56:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, From an FT Optix perspective, is it acceptable to configure 60 M850 controllers over EtherNet/IP? ------------------------------ Soumen ------------------------------
Posted By Haldar May 16, 2026 02:12:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
For one of our projects, we will be using 60 units of the Micro850 PLC Controller, all communicating with an FactoryTalk Optix PC-based runtime application. Each controller will be equipped with 5 units of 2080-SERIALISOL modules. Each 2080-SERIALISOL module will be connected to 10 Modbus RS485 ...
Posted By Haldar May 11, 2026 05:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, As per below , can we get similar status for Micro 850 controller via RA Micro Controller Driver to be shown in UI and generate alarm if not available in Network. ------------------------------ Soumen ------------------------------
Posted By Haldar May 07, 2026 02:56:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, If the customer creates new users and groups at runtime while running on a PC (and not on the Optix Panel), is uploading the runtime backup and using that backup for further development the only way to retain those newly created users and groups? Or is there any other method to store/merge the ...
Posted By Haldar Apr 29, 2026 03:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
If you allocate the license. automatically entitlement key will be visible under Entitlements Tab in FT Hub/FT Optix. Note it down the key and put it in Entitlement Manager where FT Optix is installed. ------------------------------ Soumen ------------------------------
Posted By Haldar Apr 24, 2026 07:09:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, I worked around the issue by using a container web browser. I attached an HTML file that runs inside it, with a button configured to open a new tab for the WBE session of another runtime backup. This approach is working. ------------------------------ Soumen --------------------------- ...
Posted By Haldar Apr 20, 2026 11:26:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi CodeAssist, Runtime 1 and Runtime 2 are currently running on PC1 and PC2 respectively. On the laptop (used by the CEO/MD), both Runtime1 (192.168.10.35:8080) and Runtime2 (192.168.10.73:8080) are saved as bookmarks. Clicking each bookmark individually opens its respective session. However, the ...
Posted By Haldar Apr 20, 2026 01:34:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Luca, The target device is a PC, not the Optix Panel where the Optix Studio backup was originally created. Just to confirm-are you suggesting that I should restore the runtime folder backup in order to make any further edits to the project (such as UI or other changes)? Please let me know ...
Posted By Haldar Apr 19, 2026 11:41:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Dear All, I'm looking for guidance or any relevant discussions on how to manage users and groups that are created during runtime and stored in the runtime folder rather than in the main backup. Specifically, is there a mechanism or recommended approach to ensure that newly created users and groups ...
Posted By Haldar Apr 18, 2026 04:08:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
We are running two independent FactoryTalk Optix runtime instances on separate PCs within the same network. Our requirement is to enable seamless cross-access between Runtime-1 and Runtime-2 using embedded web navigation, allowing users to open one runtime from the other via a hyperlink. Currently, ...
Posted By Haldar Apr 17, 2026 11:11:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Lucben / Ash, Thanks for the suggestion. Let me look on OPC UA cross sync. For LDAP/AD..any domain controller is required as client have two optix PC along with numbers of rockwell/siemens PLC in same network ? ------------------------------ Soumen -------------------------- ...