Singh
Contact Details
×
Enter Password
Enter Password
Confirm Password
Singh
Profile
Connections
Contacts
Contributions
Summary
Achievements
List of Contributions
My Content
1 to 6 of 6 total
search criteria =
ALL
5069-AENT/AENTR
Posted By
Singh
Oct 23, 2025 03:25:00 PM
Found In
Egroup:
Automation Control
\
view thread
Can the 5069-AENT/AENTR distributed IO be added to 1769-L33ER or 1756-L71 IO tree over eth/ip? I understand there is no hardware compatibility, but will eth/ip work? Thanks! -------------------------------------------
Powerflex 755 600V 22(ND) 17(HD)
Posted By
Singh
Mar 17, 2025 06:14:22 PM
Found In
Library:
Drives, Motion Control and Low Voltage Products
Powerflex 755 600V 22(ND) 17(HD)
Posted By
Singh
Mar 17, 2025 06:14:00 PM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Experiencing a weird issue with two Powerflex 755 drives behaving the same. Both drives show NOT ENABLED and P919 stop owner shows 13- Port 13 toggling on/off. Digging into the logic the P_PF755 AOI shows Out.LogicCommand_Stop being toggled which is probably why the ethernet command is coming in. Can't ...
RE: AB SMC Flex Soft Starters
Posted By
Singh
Jun 26, 2024 10:13:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Thanks for the response, Ashmit! I trended the hold last state reference setpoints (#21 and #22) on the 20-COMM-E card during the process of switching modes and it tends to stay at 3 (hold last state value). I think it is something in the PLC that is sending it a stop command on the first scan as ...
RE: AB SMC Flex Soft Starters
Posted By
Singh
Jun 14, 2024 10:06:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Thanks for the quick response, Ryan. I do have Parameter 22 - [Idle Flt Action] set to Hold Last, yet the drives still fault. Is there anything I'm missing in the P-SMCFlex AOI? A cfg bit perhaps? Thanks! DS
AB SMC Flex Soft Starters
Posted By
Singh
Jun 14, 2024 07:54:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Using SMC flex soft starters to run a set of 72" exhaust fans. The soft starts are parameterized using CCW and integrated with an L72 processor using datalinks and plant pax objects and AOIs. Parameter 21 (Comm Flt Action) on 20-COMM-E card on soft start is set to "Hold last." Problem: Fans stop ...
Copyright � 2026 Rockwell Automation. All rights reserved.
Powered by Higher Logic