List of Contributions

Kazuo Kondo

Contact Details

Kazuo Kondo


My Content

1 to 6 of 6 total
Posted By Kazuo Kondo Jun 18, 2025 03:56:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hello After checking GPU driver, it looked outdated. software was successfuly running after updating GPU driver. Thanks! ------------------------------ Kazuo Kondo DENSO WAVE INC ------------------------------
Posted By Kazuo Kondo Jun 06, 2025 07:44:00 PM
Found In Egroup: Advanced Software
\ view thread
Yes I am. The USB converter that I am using is confirmed on RSLinx classic to communicate with SLC processor through DF-1 protocol. I would ask RA tech support to try to get answer.
Posted By Kazuo Kondo Jun 06, 2025 01:04:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hello I am asked from some users who is facing issue of opening Emulate3D 2025. The application cersion is 18.00.01 and 18.00.00, and the isseu is error message dialog is shown when opening "Demo3D.exe". The issue is as follows; Title :"DirectX Needs Updating or Hardware Acceleration ...
Posted By Kazuo Kondo Jun 04, 2025 08:48:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Thanks a lot for your reply. What I am still experiencing the failure is, SLC 5/03 and 5/04, where UIC and DH+ embedded type. SLC 5/05 type with embedded Ethernet works with fine. first I am using commercial USB to RS232C (F) cable, then connecting to DB9M port on SLC 5/05. I am also the ...
Posted By Kazuo Kondo Jun 03, 2025 10:18:00 AM
Found In Egroup: Automation Control
\ view thread
Hello I am facing issue to run FTLogix Echo app on Windows 10/11. The issue is, Emulator Controller cannot create on FTLogix Echo Dashboard. When selecting ACD file from computer to create Emulate project, it fails with some error message on popup. According to my investigation on FT Administration ...
Posted By Kazuo Kondo Jun 03, 2025 10:04:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, I am trying to make a communication between SLC 5/05, 504, 5/03 and FTOptix App on Windows. I have confirmed SLC5/05 processor via Ethernet and serial were able to get file value from processor memory. Then, I just change processor from 1747-L553 (Enet) to L542 (DH+) and change CPU type on RSLogix ...