List of Contributions

Crouch

Contact Details

Crouch


My Content

1 to 15 of 15 total
Posted By Crouch Sep 30, 2025 09:42:00 PM
Found In Egroup: Automation Control
\ view thread
Noticed a weird quirk this morning - I have a Panelview 800 that has a couple of special user screens. I was logging into one of the user accounts and while entering the password, got an alarm. The alarm banner was on the top of the screen, behind the login inputs and the keyboard. The screen acted like ...
Posted By Crouch Sep 02, 2025 05:05:00 AM
Found In Egroup: Automation Control
\ view thread
I have a few existing processes that are controlled with SLC5/05 PLCs. We use Panelview 800 for the HMI's. Since FW 8.011 does not support the SLC5, I've been forced to keep CCW 21.00 and cannot upgrade to 21.01 or 22.00. I have acquired a new process at a remote site and am using a cellular VPN to make ...
Posted By Crouch May 30, 2024 12:51:00 PM
Found In Egroup: Automation Control
\ view thread
Hello, I have several PV800's on my site - the one I'm having a problem with is connected to a SLC5/05 over ethernet. At some point in the past, the alarm banner worked, and then it stopped working, and finally, apparently "a few months" later, the operators told me. I looked at it and the CCW file ...
Posted By Crouch Apr 04, 2024 11:36:00 AM
Found In Egroup: Automation Control
\ view thread
That was it. I was writing it to DINT, not INT. Thanks!
Posted By Crouch Apr 04, 2024 11:03:00 AM
Found In Egroup: Automation Control
\ view thread
I had tried that but assumed it was wrong because it gives an "Illegal command from local processor" error. What would cause that?
Posted By Crouch Apr 04, 2024 10:00:00 AM
Found In Egroup: Automation Control
\ view thread
I've scoured the search results here and elsewhere on the internet but can't seem to find an answer. I have a new 1756-LE24ER-QB1B that I need to read data from an SLC5/05. This is my first compactlogix development, so it's very likely that I've gotten something wrong... My IP for the compactlogix is ...
Posted By Crouch Jan 12, 2024 08:10:00 AM
Found In Egroup: Legacy
\ view thread
Thanks. Is there a way to install CCW 21.00 and 21.01 on the same machine? This hmi uses a micro850, so I can use it with 8.11 on it, but I have to maintain the other HMIs that run the SLC5s ------------------------------ Crouch ------------------------------
Posted By Crouch Jan 11, 2024 03:58:00 PM
Found In Egroup: Legacy
\ view thread
I have a panelview 800 that has firmware version 8.11 installed on it. I need to downgrade to 7.11. I have to run CCW 21.00 / FW 7.11 because I use several SLC5/05 PLCs and need to maintain connectivity, and CCW won't allow versions 21.00 and 21.01 to be installed on the same machine. When I attempt ...
Posted By Crouch Nov 22, 2023 01:56:00 PM
Found In Egroup: Automation Control
\ view thread
I have a Micro850 (2080-L50E-48AWB) and CCW Developer edition, v. 21.01. I am trying to setup a pulsed input from a flowmeter. All the examples I can find online of the high speed counter use the HSC block, but it is not listed in my HSC submenu (just HSCE, HSCE_CFG, HSCE_CFG_PLS, HSCE_READ_STS, and ...
Posted By Crouch Jul 25, 2023 03:30:00 PM
Found In Egroup: Automation Control
\ view thread
It is already flashed to 10.011, so I don't think that issue is the problem. There have been 3 previous faults like this; but they were all associated with power blips. We currently have 2 UPSs powering our power supplies, so I don't think that's the issue, either. When we had the fault the other day, ...
Posted By Crouch Jul 25, 2023 02:22:00 PM
Found In Egroup: Advanced Software
\ view thread
When I test the connection from FT TM, I get this error: But the Log in MSSQL shows: Back in FT TM, I can (despite the error when testing) click the apply button, and I get this error: There is no new entry in the MSSQL log for that. I cannot change any settings ...
Posted By Crouch Jul 25, 2023 07:13:00 AM
Found In Egroup: Automation Control
\ view thread
Yes. The safety relay has been in service for a few months now. ------------------------------ Crouch ------------------------------
Posted By Crouch Jul 24, 2023 01:43:00 PM
Found In Egroup: Automation Control
\ view thread
I have a Guardmaster 440C CR30 safety relay that I am occasionally getting a fault on: (Type 05) Internal Safety Synch Fault (Code 01) Compare UART data during operation I have gotten this twice before with the power failures, but got it just now during normal operation. What would cause ...
Posted By Crouch Jul 24, 2023 01:32:00 PM
Found In Egroup: Advanced Software
\ view thread
All my permissions in MSSQL look right. When I test the connection from the transaction manager, I can see in the MSSQL log that it is giving permission to the user to access the database, but I'm not getting any indication from transaction manager that anything is working. ------------------------------ ...
Posted By Crouch Jul 11, 2023 08:28:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, I am trying to move our process historian over from our old Windows 2000 server running RSSQL to a Windows 2019 server with FactoryTalk transaction manager. I've got MSSQL 2019 Express running, and I've transferred the old process data over into a new database on the newer server. I just can't ...