List of Contributions

McKinley

Contact Details

McKinley


My Content

1 to 20 of 22 total
Posted By McKinley Oct 07, 2025 07:31:00 AM
Found In Egroup: Advanced Software
\ view thread
Not willing to buy more licensing or use FT Link Gateway. Looking for other options. ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Oct 06, 2025 06:55:00 AM
Found In Egroup: Advanced Software
\ view thread
Trying to migrate away from RSClassic fully to FTLink. But some of the PCs still need the DDE topic function in excel for commissioning and start up. What options are available to replace this? I read somewhere that FTGateway still uses DDE but looking to move away from DDE altogether. Are there any ...
Posted By McKinley Oct 06, 2025 06:38:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks, Shane. I will keep playing with. ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Oct 01, 2025 11:09:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I understand that the SVG file is being modified outside of Optix then imported into the web browser window. It's not as smooth as I would like it and with it glitching every so often (starts back at the beginning and then jumps to where it needs to be). Even after adjusting the the duration time and ...
Posted By McKinley Sep 24, 2025 06:04:12 AM
Found In Library: FactoryTalk Optix
Posted By McKinley Sep 24, 2025 06:04:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
If you can wait a few months. RA should be releasing a lab on this. I didn't see it in the hands-on labs list for AF 2025. But be on the lookout for something called Data Ready OEE library. It's mostly smart object based but will go into detail about the full gauge object used. ------------------------------ ...
Posted By McKinley Sep 12, 2025 05:49:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you Shane, I need some time to process this. ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 10, 2025 05:38:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Shane, Do you want the position to be inputted as 0 to 400, 100 to 500, or 0 to 100% (from left)? This would be a variable. Do you want the animation duration to be fixed or variable? Animation would be ON, set by a BOOL. Do you want the animation to automatically occur when the variable ...
Posted By McKinley Sep 09, 2025 12:48:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Is the Studio application only on a laptop? What external device are you trying to view it on? ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 09, 2025 05:34:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
If I heard correctly, redundancy maybe supported when FT Optix for SCADA is released (Q1 2026). ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 09, 2025 05:08:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Does your Studio v32 application have any SFC subroutines? ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 09, 2025 05:00:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 05, 2025 05:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
What platform are you trying to see this on? ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 04, 2025 02:16:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks but need more help than that on NetLogic, have 0% C# experience. Where can I find it? ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 04, 2025 11:20:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I got the SVG working in the web browser like it should. Just need to know how to tie the variable into it with Optix. ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 04, 2025 11:19:30 AM
Found In Library: FactoryTalk Optix
Posted By McKinley Sep 04, 2025 09:55:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I originally wrote my question a couple of times, finally landing on the simplest one. Adding a variable to the SVG's left margin attribute moves the SVG as I had asked and I can make this work with multipliable SVGs. But I should be able to do this to any id/element within the SVG from the properties ...
Posted By McKinley Sep 04, 2025 04:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
How do I link the id/element to margins? ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Sep 03, 2025 07:27:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
How do you move an SVG horizontally or vertically with a variable? I'm not founding any horizontal or vertical position attributes like in FT View. ------------------------------ Regards, RYMC ------------------------------
Posted By McKinley Jul 29, 2025 05:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I believe what you are referring to is the state definition and monitoring On/Off tags. If GuardianAI would write to a drive tag when an alert happens, I could make that work. But not with the current GuardianAI controller connection setup. ------------------------------ Regards, RYMC ------ ...