List of Contributions

Automatic Insulin

Contact Details

Automatic Insulin


My Content

1 to 13 of 13 total
Posted By Automatic Insulin Apr 25, 2023 10:39:00 AM
Found In Egroup: Networks
\ view thread
Hello Scenario: Using a Stratix 5800 1783-MMS10 as Layer 2 with L2NAT for automation equipment: Is there any performance or functionality differences between using the SFP ports (1-2) with 1783-SFP1GTE (RJ45 copper 1G), or any of the other ports (3-10) as the connection up to layer 3 (Will have 2 ...
Posted By Automatic Insulin Feb 17, 2023 06:48:00 AM
Found In Egroup: Networks
\ view thread
Any luck getting some information on this? I'm in the middle of specifying for around 180 pieces of new equipment, and was going with the 5800 after being told the 5700 is going EOL. Are the 5200 series going to be less costly? More port options? ------------------------------ David --- ...
Posted By Automatic Insulin Sep 15, 2022 08:03:00 AM
Found In Egroup: Automation Control
\ view thread
Hello Dave, how long is a batch, and how accurate must the average be? Is it that the flow rate and moisture together represent the moisture of the product at that time, and it's all going into a larger container to become a complete mixed batch or product? If using ladder only, you may need to do multiple ...
Posted By Automatic Insulin Aug 10, 2022 10:10:00 AM
Found In Egroup: Automation Control
\ view thread
Hello Matt, In this case then, I recommend a cascaded loop. Loop 1 is to control the process air temp, and its output is used as the setpoint for loop2 which will control the combustion chamber temperature. The setpoint MAX for combustion chamber temperature can be your safety limit. ------------ ...
Posted By Automatic Insulin Aug 08, 2022 07:33:00 AM
Found In Egroup: Automation Control
\ view thread
It looks like with the PVEU scaling tied to the SP limits, if the actual PV exceeds PVEUMax, the results may not be as desired / expected. I think though, to answer your question more could you explain what the different temperature sensor is? i.e. load temperature? Is this an application where a cascaded ...
Posted By Automatic Insulin Oct 20, 2021 08:27:00 AM
Found In Egroup: Automation Control
\ view thread
In this case, if such an automatic login to OPERATOR is desired, I suggest creating a splash screen for power up that displays whatever information is relevant to the project/equipment. Put an "OK" or "CONTINUE" button there that does the login of the user name you want other than the "DEFAULT" - ...
Posted By Automatic Insulin Aug 03, 2021 07:09:00 AM
Found In Egroup: Networks
\ view thread
This is what I have so far, with not a single line drawn to show topology. I have these devices grouped by Line and Cell, and all these were found using the discovery tool, but the "Discover Topology" button has done nothing. What is it I am missing that I cannot get anything looking like what is shown ...
Posted By Automatic Insulin Aug 03, 2021 05:55:00 AM
Found In Egroup: Networks
\ view thread
Is there a projected release date for that? I'm actually rather disapointed with FTNM so far. I thought I would be able to build a decent network topology diagram with it, but it does not even show connection lines between devices. Am I missing something? ------------------------------ David Littlejohn ...
Posted By Automatic Insulin Aug 03, 2021 05:50:00 AM
Found In Egroup: Networks
\ view thread
Where would I add EDS files for FTNM? So far I cannot find that in the documentation. ------------------------------ AI ------------------------------
Posted By Automatic Insulin Aug 02, 2021 12:04:00 PM
Found In Egroup: Networks
\ view thread
How can you manually add details and name an unknown device in FactoryTalk Network Manager? I recently installed and am in the process of doing discovery, etc. for initial configuration, and FTNM has several items listed as device type "unknown" and will not let me change the devices to what I know they ...
Posted By Automatic Insulin Jun 30, 2021 12:29:00 PM
Found In Egroup: Automation Control
\ view thread
I'm searching for information about how updating Rockwell Software from one version to another might impact FDA guidelines regarding validated software? Specifically, we are considering upgrading FactoryTalk View ME version 9, to Version 12, and are wondering what level of re-validation is normally expected ...
Posted By Automatic Insulin Jan 21, 2021 04:51:00 AM
Found In Egroup: Automation Control
\ view thread
Hello. Thank you for the response. I need to find something more secure than this, I believe. If I understand correctly, this method would allow discovery of a user password by swiping a card to an RFID reader connected to a keylogger, or notepad running on a computer. ##HL40
Posted By Automatic Insulin Jan 20, 2021 07:19:00 AM
Found In Egroup: Automation Control
\ view thread
Summary: Login without typing user name and password Are there any methods to enable a user to login/logout of a FactoryTalk View ME application using a SmartCard or RFID badge? I'm searching for a way to leverage Windows-linked accounts to enable users to quickly login to FTVME applications without ...