List of Contributions

djorre

Contact Details

djorre


My Content

1 to 16 of 16 total
Posted By djorre Jul 26, 2013 03:01:00 AM
Found In Egroup: Advanced Software
\ view thread
Summary: Transaction Manager ODBC connector can handle only 1 stored procedure at once? Hello, This is the setup we use: FT Transaction Manager 9.00.00 CPR9 FactoryTalk Connector ODBC Connector to SQL 2005 SP1 database We have 2 Transactions. PlcToSql: ...
Posted By djorre Feb 26, 2013 10:48:00 AM
Found In Egroup: Advanced Software
\ view thread
"Supports FTHSE v2.20 on W2008 R2 Server (64 bit only): Should only be installed on this OS when FactoryTalk VantagePoint 3.1.5 needs to be collocated with it" Does that mean the same as "should only be installed if VantagePoint 3.1.5 is installed"? I think not. Even when I install ...
Posted By djorre Feb 26, 2013 10:42:00 AM
Found In Egroup: Advanced Software
\ view thread
This is my support matrix and the KB al 5 says 108387, saying you need a patch and Vantegepoint must be locally. ##HL41
Posted By djorre Feb 26, 2013 10:36:00 AM
Found In Egroup: Advanced Software
\ view thread
I installed Vantagepoint 3.1.5 and the problem persists. ##HL41
Posted By djorre Feb 26, 2013 10:24:00 AM
Found In Egroup: Advanced Software
\ view thread
The Vantegepoint revision that is on the Disk is not compatible with 2008 R2. "Otherwise it's made pretty clear that FTHSE 2.20 is not supported on a Win Server 2008 64-bit platform" No it is not, it says "KB" in stead of not supported. The KB only mentions you need to install ...
Posted By djorre Feb 26, 2013 10:17:00 AM
Found In Egroup: Advanced Software
\ view thread
But thank you for the response... I guess it is my own fault not to have checked the KB enough. Maybe I can change the batch-file and have succes afterall. Thanks anyway. ##HL41
Posted By djorre Feb 26, 2013 10:01:00 AM
Found In Egroup: Advanced Software
\ view thread
What does a Vantagepoint installation has to do with the ability to take backups using pibackup.bat? There is no Vantagepoint installed anywhere, so it is not on a remote server, so no problem! That is my logical sense in reading this KB. You think if I install Vantagepoint (that is free ...
Posted By djorre Feb 25, 2013 09:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Summary: Error on Historian backup using pibackup.bat in 64-bit environment (Program Files (x86)) Hello, Normally I configure historical backups using pibackup.bat as mentioned in the installation and configuration guide. The problem now is that this batch file fails on a system ...
Posted By djorre Aug 06, 2010 06:50:00 AM
Found In Egroup: Installation & Activation
\ view thread
I think I know what the problem was. I unchecked the 'borrow as SYSTEM user' checkbox because I had the error message: Unable to borrow RSSQLPRO.70K. Failure borrowing this activation under the SYSTEM context. You stil maybe able to borrow the activation under a normal user account. Error ...
Posted By djorre Aug 06, 2010 05:56:00 AM
Found In Egroup: Installation & Activation
\ view thread
Could it be that is has to do with the 'borrow as SYSTEM user for services' checkbox that appears when borrowing the license? ##HL62
Posted By djorre Aug 06, 2010 05:28:00 AM
Found In Egroup: Installation & Activation
\ view thread
I just tried the patch and it has not helped. This is what is in the event viewer: Logged Date: 14:23:53 Wednesday, August 04, 2010 Location: ***** Provider: FactoryTalk Activation Username: ***** Verbosity: 1 Borrowed an activation RSSQLPRO.70K 1.00 ***** from ***** for ...
Posted By djorre Aug 06, 2010 03:47:00 AM
Found In Egroup: Installation & Activation
\ view thread
Hi, My problem: 1. Installed FT Transaction Manager (CPR 9 SR 1) 2. Used it using grace period 3. Installed FT Acftivation Tool 4. Borrowed a RSSQL.70K license from our license server, using the @... this went with no problem 5. Opened transaction manager again, grace period ...
Posted By djorre Jun 29, 2009 07:21:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, I use RsBizware 7.00 with 'production server' for reporting. When I create a scheduled task in the production client than a good preview is visible of the report. But when te task runs and creates the .csv file, only the headers of this query/report are in it, no data! I have tried with printer ...
Posted By djorre Mar 19, 2009 05:23:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, I got a problem and I just can't solve it tried everything so I ended here. If I start the rsBizware Enterprise Manager, I am asked to register a Server Manager. I choose Yes and enter the hostname. Then the tree appaers with a red traffic light at 'Server Manager on (host)', I click ...