List of Contributions

Torssell

Contact Details

Torssell


My Content

1 to 8 of 8 total
Posted By Torssell Jun 03, 2026 08:44:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
For Manual 1, check page 11 for the part number. You can then use ProposalWorks or Advisor to pick out a new PowerFlex 755TS or PowerFlex 753 depending on needs.
Posted By Torssell Dec 05, 2025 02:26:00 PM
Found In Egroup: Automation Control
\ view thread
I would check PCDC and make sure you have the latest AOPs. My guess is that some drives were done with a newer firmware. -------------------------------------------
Posted By Torssell Dec 05, 2025 08:16:00 AM
Found In Egroup: Automation Control
\ view thread
You have a datalink for DC Bus Voltage on those drives. If you click on the Add On Profile, then click Overview, then click Device Definitions, and then Connection Format you get the Datalinks on that drive. Datalinks are used to transmit additional data. It's faster than using messaging. -------- ...
Posted By Torssell Nov 21, 2025 11:02:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Ahhh, that makes sense. Are there any plans to add an Application Example folder like with the Device Object Libraries? I was hoping for a quick test run of the library. I can take a closer look and use the templates to setup a demo project for myself in the mean time. ----------------------------- ...
Posted By Torssell Nov 21, 2025 10:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi @AutomateSHANE, I tried running it in the C Drive and ran into the same issue. The emulator opens, but defaults to a grey screen without any menus or buttons. -------------------------------------------
Posted By Torssell Nov 20, 2025 03:05:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi, Has anyone had any success with getting the new FactoryTalk Optix DataReady library sample project working? I'm getting this error. I updated to the most recent version of Optix Studio and ran the Setup.cmd. Any suggestions? -------------------------------------------
Posted By Torssell Jul 28, 2025 08:23:00 AM
Found In Egroup: Advanced Software
\ view thread
To add into this, if you are using Rockwell VFDs there are some VFD AOIs also. If it's PlantPAx 4.XX then you need to use P_PF52x or P_PF75x. If it's PlantPAx 5.xx then you need to use P_VSD (ideally with the power device library (found on PCDC( Rockwell's download center))).
Posted By Torssell Jul 23, 2025 08:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
See release notes for version 1.03.00 . You can use the controller tags to send up to the HMI/SCADA system from the PLC. I haven't used it myself so you might need to work with tech support to get it setup correctly. I would check with tech support if third party PLCs work or if you need to use Rockwell. ...