List of Contributions

kurt klingbeil

Contact Details

kurt klingbeil


My Content

1 to 20 of 50+ total
Posted By kurt klingbeil Feb 22, 2026 05:28:00 PM
Found In Egroup: Automation Control
\ view thread
Modbus has a couple of variants / mutations 0-based registers. (programmers unafraid of 0) 1-based addresses. (BASIC programmers) Documentation is often sloppy and imprecise Offsetting by +/-1 is the solution
Posted By kurt klingbeil Dec 15, 2025 06:47:00 PM
Found In Egroup: Automation Control
\ view thread
I remember in the 70s ... code-bashing on PDP-11 rocker switches using the OP-code reference card and then being amazed at coding FORTRAN on punch cards - a room full can sound like a machine gun shootout and early early single-board micro computers with assembly and/or some other compiled languages ...
Posted By kurt klingbeil Dec 14, 2025 02:31:00 PM
Found In Egroup: Automation Control
\ view thread
Fascinating... Does this mean that prior to Studio 5000 there was NO "tag based addressing" ? Does that imply that all prior generations were in the same league as assembly-hackers programming in octal or the incomprehensible-but-functional coding fetishes ? For get about "thinking long term"... ...
Posted By kurt klingbeil Nov 19, 2025 02:04:00 AM
Found In Egroup: Installation & Activation
\ view thread
After download the installation files I noticed one email which had an activation code When I clicked the button It generated an Activation certificate which I downloaded In the downloaded installation file pile in C:\RA - which I moved to D:\RA_Echo since there was already a D:\RA folder from ...
Posted By kurt klingbeil Nov 18, 2025 12:59:00 PM
Found In Egroup: Installation & Activation
\ view thread
I have developed a Project based on CompactLogix 5069 controller and associated IO Red Lion G15/G10 are used as the HMIs (and modbus gateway) While I had access to the hardware testing / tweaking / confirmation was straightforward Now that the hardware is field deployed, I can continue to ...
Posted By kurt klingbeil Nov 18, 2025 11:01:00 AM
Found In Egroup: Automation Control
\ view thread
I have developed a Project based on CompactLogix 5069 controller and associated IO Red Lion G15/G10 are used as the HMIs (and modbus gateway) While I had access to the hardware testing / tweaking / confirmation was straightforward Now that the hardware is field deployed, I can continue to ...
Posted By kurt klingbeil Aug 19, 2025 12:55:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
One approach for critical interlocks is to use hard-wired digital signals All of the fancy fly-by-wire stuff is cool and all, but may not be a suitable alternative to inter-connected digital IO direct programming within the drives as the primary channel with the comms channel as a backup ...
Posted By kurt klingbeil Aug 11, 2025 01:19:00 PM
Found In Egroup: Automation Control
\ view thread
I built an application in RSLogix 5000 36.11 which uses RedLion G10/G15 HMI It has been successfully field commissioned and tweaked and is operational. Some additional tweaks are in order as well as the addition of 2 actuated valves. In the absence of any hardware ... is there any way ...
Posted By kurt klingbeil Nov 11, 2024 01:05:00 PM
Found In Egroup: Automation Control
\ view thread
Thank you fuzzy logic for your response... It appears that once I have done the reply->make best answer, I can no longer reply to that message. It turns out that we are using a 5380 CompactLogix with RSLogix 5000 v36.00.00 so that Data Preserved Download should already be available ...
Posted By kurt klingbeil Nov 05, 2024 11:38:00 PM
Found In Egroup: Automation Control
\ view thread
I have poked at this before but am still uncertain about it... When I was developing this application, I simply went online and then downloaded the code for each iteration While one is connected and has made changes to tags, and one does a save, one has the option of uploading the tags which ...
Posted By kurt klingbeil Nov 05, 2024 11:26:00 PM
Found In Egroup: Automation Control
\ view thread
I just decided to do a DIY for such a trivial calculation; I found the Zeller algorithm online and just banged together this chunk of ST I didn't bother to turn it into a function since I was using it for "today" and not for arbitrary dates //Zeller DoW algorithm Zeller_year := SystemTime[0]; ...
Posted By kurt klingbeil Nov 01, 2024 03:02:00 PM
Found In Egroup: Automation Control
\ view thread
Yikes and Sheesh! What a dummy! I got confused by all the parentheses and assumed it was a function rather than an operator. Thanks a lot!
Posted By kurt klingbeil Oct 31, 2024 03:24:00 PM
Found In Egroup: Automation Control
\ view thread
Where is MOD as in Modulo ? In RS5k.. Lite Everywhere I look it just states MOD() as if it is ubiquitously present... Doesn't refer to libraries or AOI or anything. When I code it, compiler flags it as unknown function error. So what secret Masonic Handshake is required to implement such ...
Posted By kurt klingbeil Oct 07, 2024 02:00:00 AM
Found In Egroup: Automation Control
\ view thread
Having implemented the anti-windup logic, We notice that when the VFD shuts down due to LALL being reached, The PID will continue to ramp up - eventually to pedal-to-the-metal. I must be missing something... Allegedly when WindupHIn and WindupLIn are asserted CV is supposed to remain static. NSR_1010A ...
Posted By kurt klingbeil Oct 07, 2024 01:45:00 AM
Found In Egroup: Automation Control
\ view thread
Adding over-pressure protection to Level Controlled Pumping System I'm trying to wrap my head around what feels like should be a straightforward proposition. We have established reasonable control over a water pumping system using PLC-based PID reservoir level control driving VFD speed. ...
Posted By kurt klingbeil Oct 07, 2024 01:30:00 AM
Found In Egroup: Automation Control
\ view thread
We determined the minimum VFD frequency required to overcome the static pressure and set the CV control range to Hz_Min to 60Hz Is that essentially equivalent to pushing Static_Pressure_Level-equivalent into FF ? Or is that fundamentally different ? On the subject of incorporating pump curves into ...
Posted By kurt klingbeil Oct 07, 2024 12:37:00 AM
Found In Egroup: Automation Control
\ view thread
Thank you for your reply... Some advice I obtained was that it was not possible to have multiple versions of Studio5000 installed concurrently Our experience was that after having installed v37.00.00, we subsequently downloaded the v36.00.01 installation files and magically the right ...
Posted By kurt klingbeil Oct 03, 2024 09:59:00 PM
Found In Egroup: Automation Control
\ view thread
From examining several "bumpless transfer" examples I came up with this: Seems to me that OperManualReq + CVOper is similar in nature to CVInitReq + CVInitValue I would have thought that being held in Manual should have stopped windup. My guess is maybe that because the PIDE is running continuously ...
Posted By kurt klingbeil Oct 03, 2024 01:58:00 PM
Found In Egroup: Automation Control
\ view thread
I have been using RSLogixStudio5000 v 36.00.00 for several months the current revision on the CompactLogix PLC is 36.011 Now our field technician is installing RSLogixStudio5000. The same download-by-serial number has directed him to download v37.00.00 I forsee a potential cluster-beep ...