List of Contributions

de Jager

Contact Details

de Jager


My Content

1 to 9 of 9 total
Posted By de Jager Jun 12, 2024 03:38:00 AM
Found In Egroup: Advanced Software
\ view thread
That was one problem. Our company are using Cybereason (ransomware) and it is killing Factory talk services platform 6.3 and even worse 6.4. 6.3 you can just repair Factory Talk Linx after startup and all fine. 6.4 totally breaks.
Posted By de Jager May 24, 2024 08:03:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi. So I had a problem running FTView Studio for the last 3 weeks. Was working on it one day and about a week later when I needed to work on it again, it just stopped working. Starting looking everywhere for a solution to the problem and countless times of rebuilding the laptop from Windows 10 to Windows ...
Posted By de Jager Apr 22, 2024 01:56:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi @Akhilesh thanks for the reply. I ended up using the same TagTable and StringTable but separate FloatTables. In the SQL server I created a couple of Views to display data from specific tags in a datagrid. Splitting the data helps with keeping the size of the table lower so the SQL view can execute ...
Posted By de Jager Apr 22, 2024 01:45:00 PM
Found In Egroup: Automation Control
\ view thread
Hope this will help someone with the same problem. I have a couple of 1734-AENTR remote IO's on our network. All run on our network with managed switches. A while back started to notice that some of the units will fault on the ethernet side and will only reset after powering down and up again. By accident ...
Posted By de Jager Apr 22, 2024 10:57:00 AM
Found In Egroup: Advanced Software
\ view thread
Just an update on this issue. Found that the problem was caused by Regional settings on the server, decimal symbol must be "." not "," and one need to set the App properties to run as Administrator.
Posted By de Jager Apr 22, 2024 10:56:54 AM
Found In Library: Advanced Software
Posted By de Jager Apr 09, 2024 08:42:00 AM
Found In Egroup: Advanced Software
\ view thread
I Know this is an old post, but want to add some info. I did it as explained and worked like a dream and the suddenly I started getting the error in the image. Maybe Rockwell can test and update the tool to work again. Maybe need to be tested with the latest SQL versions.
Posted By de Jager Apr 09, 2024 12:49:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Rockwell at some point back supplied this DatalogDataMergeTool to do offline datalog merging. I have been using it for some time, but getting errors lately. Don't know if the problem is with the tool or the SQL version. Attached is an image of the error I get. Hope someone has a solution for ...
Posted By de Jager Apr 04, 2024 11:23:00 AM
Found In Egroup: Advanced Software
\ view thread
If I create two datalog models, one for periodic logging and another for on change logging and both are logging to the same SQL odbc database, do I use the same tables in both datalog models, or do I create separate tables for each model?