List of Contributions

Ali

Contact Details

Ali


My Content

1 to 20 of 20 total
Posted By Ali Feb 01, 2024 12:48:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Philip, Thanks for the quick response. Our concern is that under a comms trip, there is no visible way for an operator in the field to know via the diagnostic unit (HMI) that there has been a comms fault. Is this to be expected? It is only being understood that there is a comms ...
Posted By Ali Jan 31, 2024 10:44:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Philip, can you please advise how we can set E300 to go trip state on Communication fault? we can set the output points open/close on Comms fault but E300 not going to trip state .
Posted By Ali Jan 23, 2024 10:29:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Gi Gents. We controlling a PowerFlex755 drive with a 20-COMM MODBUS TCP module. we set the speed ref to the 20-COMM module (Port-6 parameter#930) and can see the set speed value at parameter 876. But somehow can't see anything on the main control board speed commanded value parameter# 2. ...
Posted By Ali Jan 21, 2024 10:51:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
we checked in Run mode it's still the same issue, not getting anything on holding registers. ------------------------------ Ali ------------------------------
Posted By Ali Jan 21, 2024 07:47:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Phil, can you please advise how can set it to Run mode through the Anybus module? At the moment rotary switches at 0.0.0 when I changed it just lost the Set IP after a power cycle. Thanks. ------------------------------ Ali ------------------------------
Posted By Ali Jan 21, 2024 06:33:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Phil, we getting data on Input registers 30013-30014-30015, but nothing on Holding Registers 44023-44024-44025 even after Firmware update. Thanks. ------------------------------ Ali ------------------------------
Posted By Ali Jan 19, 2024 04:17:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Philip, We tried that but no luck yet, do you have idea how we can update firmware of AnyBus E300 ModbusTCP? Any help would be appreciated, we really stuck at this point. Thanks ------------------------------ Ali ------------------------------
Posted By Ali Jan 18, 2024 04:40:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Philip, Web server showing the correct live data from E300. but issue is we not getting any thing in Modbus register. Ww already connected Anybus, they saying it's Rockwell side issue. ------------------------------ Ali ------------------------------
Posted By Ali Jan 18, 2024 03:51:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Philip, Modbus read request is ok, no comme error. 44022 reading the data (2 Bytes) ,but data in 4403-4404 not changing just showing the Zero values . ------------------------------ Ali ------------------------------
Posted By Ali Jan 18, 2024 03:07:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, we are using AnyBus E300 Modbus TCP module, we have comms working and can control the E300 using Modbus commands. We are facing an issue while reading the E300 L1 current reading at the moment we can only read the E300 Avg FLA % data (Anybus Modbus register: 44022), the remaining registers just ...
Posted By Ali Jan 18, 2024 03:06:29 AM
Found In Library: Drives, Motion Control and Low Voltage Products
Posted By Ali Nov 16, 2023 06:17:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Daniel, Yes, it happens every time power up and make drive enable. For your reference, only power up the control module using 24V DC. Parameter 189 = Disabled Parameter 321 = Disabled Parameter 450 = Coast Parameter 454 = 180.00VDC Thanks ---- ...
Posted By Ali Nov 16, 2023 12:10:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, What could be the reason for Precharge Open Alarm on PowerFlex753? Try to disabled the Precharge in Parameter#190 but still get the Alarm on Power up. Alarm code 138. Attached is the configured VSD. Thanks. ------------------------------ Ali ---------------- ...
Posted By Ali Nov 16, 2023 12:09:35 AM
Found In Library: Drives, Motion Control and Low Voltage Products
Posted By Ali Nov 15, 2023 01:37:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, I'm using a 20-comm-M Modbus/TCP module with a PowerFlex 753 drive and want to test Modbus parameters using the emulator. But unable to establish a connection with the 20-Comm-M adaptor. Does anyone know what parameters should be checked to establish Modbus comms ?? Thanks ...
Posted By Ali Oct 24, 2023 10:15:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Can we configure Driver parameters through 20-COMM-M MODBUS/TCP ADAPTOR, or do we need a USB cable to connect the PowerFlex 753 drive to CCW? ------------------------------ Ali ------------------------------
Posted By Ali Oct 24, 2023 08:12:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, Is that possible for us can set PowerFlex 753 parameters through 20-COMM-M Modbus/TCP Adaptor, Adaptor Manual believes only can access Modbus/TCP parameters. If we can't access the parameters through 20-COMM-M Modbus/TCP Adaptor, do we need a USB cable to connect the drive using CCW? ...
Posted By Ali Oct 24, 2023 12:26:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, Is it possible to only power up the control module of PowerFlex 753, if we don't have access to a 3-phase supply? Just only want to test the comms. Thansk. ------------------------------ Ali ------------------------------
Posted By Ali Oct 05, 2023 07:33:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Daniel, Yes, we want to configure it as a Trip relay, like we can configure "Trip Relay' in the central control module and it changes state when E300 tripped. can we do the same with expansion module output relays? if so which parameters need to be set . Thanks -------- ...
Posted By Ali Oct 05, 2023 04:27:00 AM
Found In Egroup: Automation Control
\ view thread
Can I use an Ouput relay from a E300 Digital Expansion IO module as a Trip Relay? EDIT: moved to Automation Control community -FL ------------------------------ Ali ------------------------------